Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Car Media Centre Idea
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 42 subscribers
  • Views 593 views
  • Users 0 members are here
  • Single Board Computer
Related

Car Media Centre Idea

mrb23
mrb23 over 10 years ago

A project I think would be a cool design challenge and that I would find useful would be an in car media PC. Ideally based on raspberry Pi! A device that looked good and allowed the integration of modern media features into older cars would be awesome!

 

I envisage it using a custom printed case that could attach to the heater vents in most cars with a separate, ergonomically designed controller housing so that it can be operated more comfortably than reaching up to touch the unit (this would also make it less likely that the unit would be knocked off it's mounting)

 

To be really useful it would:

- run off the car's 12v supply (cigar lighter socket?)

- small internal battery to prevent blackout/brownout if car supply drops (ie during starting engine)

-low power mode to allow adding/removing media when car is off without draining battery

- custom rotary controller (similar to iDrive/MMI controllers) to operate, could be touchscreen instead (also??) but that would lead to finger marks on display and increase cost

- analog audio out to pipe into car stereo

 

Other features that would be desirable:

- WiFi enabled to allow managing media from inside home

- FM radio audio output to play over car speakers if no audio in available

- blutooth connectivity to answer phone calls

- leverage OBDII port in modern cars to get data from ECU ( possibly be able to read/clear fault codes)

- be able to add satellite navigation or DAB/DVB if desired

- allow connection of other audio devices or media storage via usb

 

This is is something I have wanted to see done for ages and any attempts at in car PCs I can find online are really let down by case design and the lack of a controller that isn't the touchscreen!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +1
    I was literally just about to suggest the same. As well as OBDII functionality, maybe some CAN bus integration to control car functions and build custom gauges etc.
  • e14 Contributor
    e14 Contributor over 10 years ago

    I was literally just about to suggest the same.

     

    As well as OBDII functionality, maybe some CAN bus integration to control car functions and build custom gauges etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mrb23
    mrb23 over 10 years ago in reply to e14 Contributor

    CANBUS would be awesome!

     

    The he whole idea came to me when I wanted to add some music to my iPod and realised I'd left it in the car!