Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Super-flexible USB charger
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 40 subscribers
  • Views 181 views
  • Users 0 members are here
  • Single Board Computer
Related

Super-flexible USB charger

tinue
tinue over 11 years ago

I have a bench power supply, that can handle 0-30V up to 5A. It's simple to construct a cable that allows me to connect an USB Type A female plug to the bench supply (or directly a male Micro USB B, or whatever).

 

However, this will not charge anything with more than 500mA. To let the to-be-charged device know that it can pull more current (or voltage), one of the many signaling standards must be used:

  • Fixed voltages on D+ and D-
  • USB Battery Charging Specification 1.1 or 1.2
  • USB Power Delivery specification
  • Qualcomm Quick Charge 2.0 or 3.0

 

What I would like to see is a universal device that can signal using any of these standards downstream. For the signaling and UI part a micro controller should be used. Voltage regulation and current limitation must also be built. Possibly more than one downstream port could be provided, each one individually controlled.

The actually used D+ and D- values should be displayed; The actual voltage and current as well, plus both integrated over time (to measure e.g. how much mAh go into a power bank in what amount of time).

A subset of this functionality is available in the form of various "YZX Studio" USB Power Meters, by the way.

 

The device can be used as a simple charger, but would also be very useful for testing purposes.

I can't build one of these, so this is merely an idea for a project image