Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Solar Powered Raspberry Pi Setup
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 41 subscribers
  • Views 374 views
  • Users 0 members are here
  • Single Board Computer
Related

Solar Powered Raspberry Pi Setup

escape86
escape86 over 9 years ago

Something I've always thought would be cool is a solar-powered setup for single board computers. Something like an Arduino could run for a while off of batteries, but what about having something like a Raspberry Pi running 24/7 with only a solar panel and battery as a power source? Anywho, I love the show! Keep up the great work!

  • Sign in to reply
  • Cancel
Parents
  • newbreed2001
    newbreed2001 over 9 years ago

    I'm actually working on this right now. Still working on the 24x7 part, but I have all the components and just need more time testing and tweaking. I have a Raspberry Pi 3 Model B with a Element 14: 4DPi-24-HAT (Raspberry Pi 2.4in QVGA Touchscreen LCD Hat Module) running on off a 7800 mAh battery pack with 2.5 amps & 5 volts output. My portable solar panel is still being tested out on sunny days image to confirm if size will keep up with charging rate requirements. You do need a large enough battery with a charge pass-through feature to allow charging of the cells and USB power output at the same time.

     

    My Pi 2 has much lower power requirements, but does not have WLAN to be fully wireless & mobile (and is currently used for my Cacit server). It will be running from a buck converter off 12v battery setup once my larger PV panels are setup. That will be running headless 24x7 gathering charge controller stats. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • newbreed2001
    newbreed2001 over 9 years ago

    I'm actually working on this right now. Still working on the 24x7 part, but I have all the components and just need more time testing and tweaking. I have a Raspberry Pi 3 Model B with a Element 14: 4DPi-24-HAT (Raspberry Pi 2.4in QVGA Touchscreen LCD Hat Module) running on off a 7800 mAh battery pack with 2.5 amps & 5 volts output. My portable solar panel is still being tested out on sunny days image to confirm if size will keep up with charging rate requirements. You do need a large enough battery with a charge pass-through feature to allow charging of the cells and USB power output at the same time.

     

    My Pi 2 has much lower power requirements, but does not have WLAN to be fully wireless & mobile (and is currently used for my Cacit server). It will be running from a buck converter off 12v battery setup once my larger PV panels are setup. That will be running headless 24x7 gathering charge controller stats. image