Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum More Engine Management
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 41 subscribers
  • Views 1282 views
  • Users 0 members are here
  • gasoline_engine_management
  • arduino
Related

More Engine Management

jack.chaney56
jack.chaney56 over 8 years ago

In the previous discussion, I presented a base system for engine management. The problem with what was created is, it only runs in steady state. Steady state for an engine is constant rpm and load, no acceleration, and no change to demand. The software components of the system have been intentionally designed to be independent of hardware processor. The specific platform is the Arduino Nano and the 328p processor. The choice was as an exercise to see if it could be done, and to force a level of discipline for the programming model. The other item of note from the previous discussion is, I am a software person primarily, with a working knowledge of electronic hardware. I am happy to admit to shortcomings in any circuits that I present, and encourage correction.

 

This second section will deal with making improvements to the basic software to manage the asynchronous events. Some items will make reference to the previous discussion, so please review for a full description. If something was left out, I am happy to fill in the detail. Jumping in to the first item which is a one time event. The engine start. When the engine is cranking, before ignition timing is captured, fuel is being input, and not burned. To correct the state, once the engine starts, the acceleration is raised temporarily to "burn off" the excess fuel. This is done by adjusting the advance, first increasing, then reducing back to steady state.  Also, during crank (before ignition capture), the advance is reduced to almost zero. Because the advance goes from near zero to a large angle, a measured transition is needed. This is called the ramp in rate. Also, the recovery from the large angle to the steady state angle, is again a measured value. This is called the decay. The startup sequence then becomes a small state operation. Crank > Ramp to max > Decay to steady > Steady State. In each of the states a value is combined as part of the total advance.

 

The ramp in and decay are governed by the RPM of the motor, so a counter tied to the cam signal is implemented. The four states are monitored with a simple switch operation. The values for ramp in and decay are defined in calibration, as well as the values for max and minimum advance. The other part is to implement a counter of some sort that is updated during the cam signal detect (same place as setting cam detected flag). The sequence works sort of like this:

  • Engine off - Retrieve from calibration values for min, max, ramp, and decay.
  • Crank to start - Set advance to minimum until ignition is detected, also set counter to ramp in value when ignition is detected change state.
  • Ramp in - Adjust advance from minimum to maximum with a slope = counter / ramp until max is reached then set counter to decay and change state
  • Decay out - Adjust advance from max to steady state with a slope = counter / decay until steady state is reached then change state
  • Steady State - watch for engine stop

 

SWord updateStartupTrim(SWord t) {
 static SWord ramp;
 static SWord min = 0;
 static SWord max = 0;
 static UByte stState = 0;
 switch(stState) {
 case 0:  // engine off, crank to start
  min = getIgnStartupAdjustment() - t; ramp = getIgnStartupRampIn(); if (ramp == 0) { ramp = 1; }
  ignStTrim = getRpm() > 0 ? min : 0;
  if (getRpm() > getIgnRpmMinRun()) { camTrimCt = ramp; stState = 1; }
  break;
 case 1:  // ramp in
  max = getIgnStartupTrim();
  if (camTrimCt > 0) { ignStTrim = max - (SWord)((SLong)camTrimCt * (SLong)(max - min) / (SLong)ramp); }
  else { ignStTrim = max; ramp = getIgnStartupDecay(); if (ramp == 0) { ramp = 1; } camTrimCt = ramp; stState = 2; }
  break;
 case 2:  // decay
  if (camTrimCt > 0) { ignStTrim = (SWord)((SLong)max * (SLong)camTrimCt / (SLong)ramp); }
  else { ignStTrim = 0; stState = 3; }
  break;
 default: // running
  ignStTrim = 0;
  if (isEngStopped()) { stState = 0; }
  break;
 }
 return ignStTrim;
}

 

The variable camTrimCt is the counter which gets decremented on each cam.

 

Good news is, there are lots of exception and asynchronous activities to manage, so there will be lots offered here

 

Jack

  • Sign in to reply
  • Cancel

Top Replies

  • jack.chaney56
    jack.chaney56 over 8 years ago +2
    Here is where I get some people upset. I generally have great respect for electrical engineers, and their capabilities to develop really good hardware solutions. I am by training a software development…
  • jack.chaney56
    jack.chaney56 over 8 years ago +1
    Should add the link to the previous discussion as well. Engine Management
Parents
  • jack.chaney56
    jack.chaney56 over 8 years ago

    Darn old work keeps getting in the way of this important stuff. Sorry for any delays for the information flow.

     

    The table operation is kind of a key element for the engine management stuff. By using a planar table where the axis are taken from RPM and MAP, the cells can be set as a value for angle of advance.  The value of MAP can actually be a direct read from the A/D because it is a 10 bit device and the range is set from 0 to 1023, and by doing a ratio conversion for RPM it too will be a value from 0 to 1023 for min/max RPM.  Elements of temperature and barometric pressure can be added a little later.

     

    I think all the parts are there now. Table size is limited to the amount of EEPROM on the device, so I used an 8x8 table for the base advance.  I used 8x1 tables for each of the sensors (MAP, Throttle position, Engine Coolant Temp, Intake Air Temp, Battery Voltage, Fuel Pressure, and O2). The rest are either simple 1x1 cell values, or bit values for on and off states.

     

    The value of dwell is a time that it takes the coil  to charge, so at run time the value is converted to an angle using the magic number BASE, where:

     

    BASE = crkDiff * teeth / PART1

     

    and the conversion from time to angle is:

     

    dwlAngle = baseDwell * PART2 / BASE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jack.chaney56
    jack.chaney56 over 8 years ago

    Darn old work keeps getting in the way of this important stuff. Sorry for any delays for the information flow.

     

    The table operation is kind of a key element for the engine management stuff. By using a planar table where the axis are taken from RPM and MAP, the cells can be set as a value for angle of advance.  The value of MAP can actually be a direct read from the A/D because it is a 10 bit device and the range is set from 0 to 1023, and by doing a ratio conversion for RPM it too will be a value from 0 to 1023 for min/max RPM.  Elements of temperature and barometric pressure can be added a little later.

     

    I think all the parts are there now. Table size is limited to the amount of EEPROM on the device, so I used an 8x8 table for the base advance.  I used 8x1 tables for each of the sensors (MAP, Throttle position, Engine Coolant Temp, Intake Air Temp, Battery Voltage, Fuel Pressure, and O2). The rest are either simple 1x1 cell values, or bit values for on and off states.

     

    The value of dwell is a time that it takes the coil  to charge, so at run time the value is converted to an angle using the magic number BASE, where:

     

    BASE = crkDiff * teeth / PART1

     

    and the conversion from time to angle is:

     

    dwlAngle = baseDwell * PART2 / BASE