Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum computer power supply with built in battery backup
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 45 subscribers
  • Views 6986 views
  • Users 0 members are here
  • Single Board Computer
Related

computer power supply with built in battery backup

mattbatt0
mattbatt0 over 10 years ago

It has always annoyed me that uninteruptible power supplies convert AC into DC then back into AC so that the computer can convert the AC back in to DC.  I always wanted an ATX style power suply that only converted AC into DC once for powering the system and charging a backup battery.  I have thought about building it myself but I don't know what the pitfalls might be. 

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 10 years ago +3
    Hi Matt, The APC supplies are set up like this because desk top computers and monitors can not run directly off a single DC voltage. The ATX power supply creates + and - 12 volts, + 5 volts, and perhaps…
  • shabaz
    shabaz over 10 years ago +2
    Another approach is to move some tasks to low-power platforms such as single board computers (SBC) - like the Raspberry Pi or BeagleBone Black. Or even a router if you can run things on it (some allow…
  • gadget.iom
    gadget.iom over 10 years ago +2
    Google took this approach with their early server builds. http://www.cnet.com/news/google-uncloaks-once-secret-server-10209580/
Parents
  • shabaz
    shabaz over 10 years ago

    Another approach is to move some tasks to low-power platforms such as single board computers (SBC) - like the Raspberry Pi or BeagleBone Black. Or even a router if you can run things on it (some allow this), or your network storage. They need a single DC low voltage power supply.

    Maybe nothing else is critical and can be rebuilt.

     

    As an example, I wanted something guaranteed to work for a couple of hours in the event of power outages (it was an experiment that needed to run for several months uninterrupted), so I provided a 12V supply to a router and to a single board computer. My supply came from eight AA alkaline batteries : )

     

    No need to worry about charging them, and they would have powered my devices for an hour or two. I used a relay to switch them : ) didn't require MOSFET switching either. The relay was quick enough combined with a bulk storage capacitor. Nice and simple. I could replace the batteries at any time (e.g. once a year, or after an outage) provided it wasn't during an outage.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 10 years ago

    Another approach is to move some tasks to low-power platforms such as single board computers (SBC) - like the Raspberry Pi or BeagleBone Black. Or even a router if you can run things on it (some allow this), or your network storage. They need a single DC low voltage power supply.

    Maybe nothing else is critical and can be rebuilt.

     

    As an example, I wanted something guaranteed to work for a couple of hours in the event of power outages (it was an experiment that needed to run for several months uninterrupted), so I provided a 12V supply to a router and to a single board computer. My supply came from eight AA alkaline batteries : )

     

    No need to worry about charging them, and they would have powered my devices for an hour or two. I used a relay to switch them : ) didn't require MOSFET switching either. The relay was quick enough combined with a bulk storage capacitor. Nice and simple. I could replace the batteries at any time (e.g. once a year, or after an outage) provided it wasn't during an outage.