element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Show Off Your Build
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 109 replies
  • Subscribers 41 subscribers
  • Views 14886 views
  • Users 0 members are here
Related

Show Off Your Build

ChristyZ
ChristyZ over 16 years ago

How to upload a Video

 

1 - On the right column, on the "Actions" box, click on "Start a discussion". The Discussion editor page will load.

2 - Once on the "Discussions" editor, give your discussion any name you want: My First Build

3 - To upload a video, click on the video icon (see image bollow) on the "Discussions" editor window

image

 

4 - Choose from where the video is going to be uploaded: from your computer, from your videos, or from the web

image

5 - Press "Submit video"

 

 

How to upload a picture

 

1 - Click on  "Insert image" icon of the "Discussions" editor

image

 

2 - On the "Inset Image" screen, follow the steps to insert your image

image

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago +2
    My son was sent to Iraq and he wanted to take his game console and laptop. The big issue for him was the shipping and the sand. He bought a Pelican brand gun case, some foam from the craft store and a…
  • e14 Contributor
    e14 Contributor over 13 years ago +2
    Halloween Costume- Insanely Geeky!! Mr Arcade Halloween Costume on youtube!! I made it! Full description is in the video description on Youtube including a quick video of how I made it!! Could you make…
  • e14 Contributor
    e14 Contributor over 16 years ago +1
    Ben Heck is pretty much my role model, ever since i saw his first 360 laptop, im 15, and ive been repairing computers and electronics since i was about 6 or 7, im great with soldering, and working with…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Here's my challenge for Ben:

     

    Dear Ben,

     

    For a while now I've been looking for a way to modify an NES Zapper to work on modern televisions. After a lot of research, i think i have figured out exactly why it doesn't work. Unfortunately, however, i am just a computer science student with only very basic experience in working with electronics, so i do not know how to even begin implementing a solution. I was hoping you would be able to help.

     

    As you probably know, the Zapper works by having the entire screen go black save for the targets, at which point a photo diode senses whether or not it is pointing into the light. However, this is actually accomplished by a multistage process which i will outline below:

     

    1) The NES redraws the screen completely black for one frame. The Zapper checks to make sure no light is detected before proceeding, preventing any accidental readings from other light sources (this is why pointing it at a light bulb doesn't work).

    2) The NES redraws the screen with only target #1 illuminated for one frame. The Zapper checks for light, and the Nintendo determines if the player has hit target #1.

    3) The NES redraws the screen with only target #2 illuminated for one frame. The Zapper checks for light, and the Nintendo determines if the player has hit target #2.

    4) This process repeats for all targets on screen.

     

    The obvious issue with modern televisions is that they tend to upscale the image, resulting in a slight delay that messes up the precise timing required for this sequence to work. Another potential issue i have read about is the nature of the photo diode itself. I have heard that Nintendo opted to use cheap photo diodes that only detect the infrared light coming from the CRT, thus preventing it from working on modern televisions, however i can not verify this.

     

    I was hoping that you would be able to come up with a creative solution to this problem that even someone as inexperienced as me would be able to follow (maybe even make an episode out of it image ).

     

    -Andrew

     

    Sources:

    https://www.youtube.com/watch?v=c3tBk-LYyzo

    nes monitor - Why doesn't Duck Hunt work on plasma or LCD screens? - Arqade

     

    EDIT: Someone on youtube has been working on a solution to this problem, but it has been a year since they last updated so i have no idea if they ever finished it. If you have any doubt that this is possible, here is a video where he shows his working prototype: https://www.youtube.com/watch?v=8D624JADDOw

     

    EDIT 2: A possible solution i have considered would be to connect to the expansion port on the bottom of the nintendo using an ENIO board to allow the gun to directly interface with the 2A03, but i have no idea how i would implement this or how it would actually work. It would probably need to tell the game to flash the targets on screen, then wait until the gun can determine whether or not it is pointing at a target before advancing to the next bit of code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Here's my challenge for Ben:

     

    Dear Ben,

     

    For a while now I've been looking for a way to modify an NES Zapper to work on modern televisions. After a lot of research, i think i have figured out exactly why it doesn't work. Unfortunately, however, i am just a computer science student with only very basic experience in working with electronics, so i do not know how to even begin implementing a solution. I was hoping you would be able to help.

     

    As you probably know, the Zapper works by having the entire screen go black save for the targets, at which point a photo diode senses whether or not it is pointing into the light. However, this is actually accomplished by a multistage process which i will outline below:

     

    1) The NES redraws the screen completely black for one frame. The Zapper checks to make sure no light is detected before proceeding, preventing any accidental readings from other light sources (this is why pointing it at a light bulb doesn't work).

    2) The NES redraws the screen with only target #1 illuminated for one frame. The Zapper checks for light, and the Nintendo determines if the player has hit target #1.

    3) The NES redraws the screen with only target #2 illuminated for one frame. The Zapper checks for light, and the Nintendo determines if the player has hit target #2.

    4) This process repeats for all targets on screen.

     

    The obvious issue with modern televisions is that they tend to upscale the image, resulting in a slight delay that messes up the precise timing required for this sequence to work. Another potential issue i have read about is the nature of the photo diode itself. I have heard that Nintendo opted to use cheap photo diodes that only detect the infrared light coming from the CRT, thus preventing it from working on modern televisions, however i can not verify this.

     

    I was hoping that you would be able to come up with a creative solution to this problem that even someone as inexperienced as me would be able to follow (maybe even make an episode out of it image ).

     

    -Andrew

     

    Sources:

    https://www.youtube.com/watch?v=c3tBk-LYyzo

    nes monitor - Why doesn't Duck Hunt work on plasma or LCD screens? - Arqade

     

    EDIT: Someone on youtube has been working on a solution to this problem, but it has been a year since they last updated so i have no idea if they ever finished it. If you have any doubt that this is possible, here is a video where he shows his working prototype: https://www.youtube.com/watch?v=8D624JADDOw

     

    EDIT 2: A possible solution i have considered would be to connect to the expansion port on the bottom of the nintendo using an ENIO board to allow the gun to directly interface with the 2A03, but i have no idea how i would implement this or how it would actually work. It would probably need to tell the game to flash the targets on screen, then wait until the gun can determine whether or not it is pointing at a target before advancing to the next bit of code.