• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum viewer challenge: a benchtop injection molding machine
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 31 subscribers
  • Views 2206 views
  • Users 0 members are here
  • viewer
  • build_challenge
  • challenge
  • ben_heck
  • show_idea
Related

viewer challenge: a benchtop injection molding machine

e14 Contributor
e14 Contributor over 15 years ago

Hi Ben,

 

So, I've seen a few youtube videos of people converting the Harbor Freight mini-mill to be CNC and I've seen the maker bot plastic extrusion 3D printer, now let's connect the dots and create a plastic injection molder.  With the HF CNC mill, one could, in theory, mill metal molds for an injection molding machine.  The maker bot guys figured out how to control the melting of plastic for their extruder.  If you put those things together, you get the basic parts of an injection molding machine.  The only thing left is a hopper fed piston type arrangement that can soften/melt the plastic and push it into the mold.

 

To me, the injection molding machine is the last unconquered territory of the homemade fabrication machines.  CNC has been done.  Circuit board reflow has been done.  Picking and placing of electronic parts has been done.  3D printing is a work in progress.  However, injection molding plastic parts is still beyond the capabilities of the average DIY'er.  To have a plastic part injection molded by a company costs a couple thousand dollars minimum.  If I had a benchtop molding machine and a CNC metal mill that could crank out molds for me, I'd be in plastic molding heaving.

 

Imagine if you could mold the shells of your game machine laptops instead of gluing/stacking/screwing CNC'd plastic parts.

 

Thanks,

Dave

  • Sign in to reply
  • Cancel
Parents
  • Ashen
    Ashen over 15 years ago

    Just to elaborate on my first reply a bit. This is the only commercial "tabletop" injection molding machine I am aware of that exists: babyplast We have one in the engineering department of the plant I work in. It makes parts about the size of a thumbscrew or smaller. To try and mold anything larger than that in said machine would just result in disaster.

     

    I should probably explain a bit how injection molding works. Injection molding machines are sold based on clamping pressure (tons) and barrel capacity (how much melted plastic can fit in the barrel in oz). Now the basic jist of injection molding is that material (plastic) is fed into the barrel of the machine where it is conveyed by a rotating screw through the barrel to the front of the screw whilst being heated to melt the plastic (90% of the heat generated to melt the plastic is shear heat and not heat generated by the electric heaters) esssentially building your "shot size" at the front of the screw. After the shot size is built in the front of the screw the screw then acts as a ram of sorts to inject the plastic into the mold. Now the best thing I can think of to compare this part of the process to is play dough. Remember when u were little and u had those play dough sets where u stuffed the play dough into a hole and then pushed it through with a ram to make spaghetti or w/e. This is about the same consistancy as melted plastic (or at least as close of a comparison as I can make). It requires tremendous amounts of pressure to push this molten crap into a mold and effectively "pack out" the part. The typical machine in my plant is 150-300 tons with barrel capacitys from 5-35 oz and the hydraulic injection pressures set on these machines can reach 10,000 - 20,000psi (this is at the ass end of the barrel, at the nozzle tip you can generally say this pressure is amplified by 10x+) This is why the clamping ends of these machine need such force to be applied to the mold halves to keep them closed during injection. without proper clamping forces you would just blow the mold open and squirt hot plastic everywhere.

     

    I wont really get into molds much as this post is probably already boring enough. But I will say that molds are generally very expensive. The cheapest mold in our plant (besides the inserts we use in our babyplast) cost us roughly $150,000. Most are probably upwards of a half a mil. Now thats not to say you cant have an cheap mold made say out of aluminum or some other cheap metal. but it probably wont hold up very long and most likely wont make you very many good parts.

     

    To put all of this in perspective, to mold say the case for a gameboy (two halves, very simple design. molded out of probably polystyrene or abs). Nintendo or whoever they contracted to mold their gameboy cases probably used at the very least a 100-150 ton molding machine with a 15-20oz barrel (about the size of a large SUV) to run a single cavity mold. To injection mold something like Ben's 360 laptop case would most likely require a 200-300 ton machine with a 20-30oz barrel.

     

    hope this was informative image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Ashen
    Ashen over 15 years ago

    Just to elaborate on my first reply a bit. This is the only commercial "tabletop" injection molding machine I am aware of that exists: babyplast We have one in the engineering department of the plant I work in. It makes parts about the size of a thumbscrew or smaller. To try and mold anything larger than that in said machine would just result in disaster.

     

    I should probably explain a bit how injection molding works. Injection molding machines are sold based on clamping pressure (tons) and barrel capacity (how much melted plastic can fit in the barrel in oz). Now the basic jist of injection molding is that material (plastic) is fed into the barrel of the machine where it is conveyed by a rotating screw through the barrel to the front of the screw whilst being heated to melt the plastic (90% of the heat generated to melt the plastic is shear heat and not heat generated by the electric heaters) esssentially building your "shot size" at the front of the screw. After the shot size is built in the front of the screw the screw then acts as a ram of sorts to inject the plastic into the mold. Now the best thing I can think of to compare this part of the process to is play dough. Remember when u were little and u had those play dough sets where u stuffed the play dough into a hole and then pushed it through with a ram to make spaghetti or w/e. This is about the same consistancy as melted plastic (or at least as close of a comparison as I can make). It requires tremendous amounts of pressure to push this molten crap into a mold and effectively "pack out" the part. The typical machine in my plant is 150-300 tons with barrel capacitys from 5-35 oz and the hydraulic injection pressures set on these machines can reach 10,000 - 20,000psi (this is at the ass end of the barrel, at the nozzle tip you can generally say this pressure is amplified by 10x+) This is why the clamping ends of these machine need such force to be applied to the mold halves to keep them closed during injection. without proper clamping forces you would just blow the mold open and squirt hot plastic everywhere.

     

    I wont really get into molds much as this post is probably already boring enough. But I will say that molds are generally very expensive. The cheapest mold in our plant (besides the inserts we use in our babyplast) cost us roughly $150,000. Most are probably upwards of a half a mil. Now thats not to say you cant have an cheap mold made say out of aluminum or some other cheap metal. but it probably wont hold up very long and most likely wont make you very many good parts.

     

    To put all of this in perspective, to mold say the case for a gameboy (two halves, very simple design. molded out of probably polystyrene or abs). Nintendo or whoever they contracted to mold their gameboy cases probably used at the very least a 100-150 ton molding machine with a 15-20oz barrel (about the size of a large SUV) to run a single cavity mold. To injection mold something like Ben's 360 laptop case would most likely require a 200-300 ton machine with a 20-30oz barrel.

     

    hope this was informative image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Ashen

    So I get your point that traditional injection molding requires massive machines and a lot of power. But some of this doesn't make sense.  If that's the only way it can be done, does that mean when a toy company makes a new toy with 50 different plastic parts that they spend $5-10 million creating the molds and molding the plastic?

     

    I can understand that you need a huge machine if you're going to use physical pressure to melt the plastic and ram it into the mold.  But what about using heat instead of brute force to melt it.  Then wouldn't you need just a simple piston type of setup to push the plastic out into the mold?  It seems like this can be done at a smaller scale without massive SUV sized industrial machines.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Ashen
    Ashen over 15 years ago in reply to e14 Contributor

    Wookie,

     

    Like I said in my first post I'm not trying to discourage anyone from trying to DIY. Only trying to shed some light on the subject of injection molding.

     

    To answer your questions. No, I also seriously doubt that most toy companies spend $100,000+ on each one of thier molds (although I do know for sure that LEGO does, they have 50+ machines in thier germany plant, all shiny new custom built arburg machines which are switched out for new every few years). What most toy companies probably do is called insert molding. Which is simply instead of changing the whole injection mold when its time to make a new part. They exchange the Core and Cavity inserts in the mold itself. In doing so they avoid the high costs of having a whole new mold built for each different piece. Also some toy companies probably use molds made out of aluminum or cheap steel contracted to be built in china (where injection molds can be machined very cheaply). But like I said before these molds probably dont hold up for any extended period of time. Some companys also use multicavity molds to mold different parts in the same shot (think all those different army men that come in a bucket for a simple example). Toy companys also dont need to worry about stringent dimensional tolerances either. Which if you were making your own 360 laptop case or something similar I'm sure would be a concern for you (since you would want the case halves to fit together nicely).

     

    Another good example I can give you is tooth brushes. You would think that something as simple as a tooth brush would be easy and cheap to manufacture but the fact is that its just not so. The fancy tooth brushes you see today with the nice "grippy stuff" (TPE or Thermoplastic Elastomer) on the handle are made in multicavity "co injection" molds with state of the art robotics to insert the brushes and to removed the finished parts. These (usually massive) machines have multiple injection units and rotary "turntables" that swing the mold into a different position for different phases of the molding cycle. All just to make a simple toothbrush. The initial investment in these machines and molds goes into the millions. For something that to the end user only costs a couple bucks. Here is a simple example of this on You-Tube: http://www.youtube.com/watch?v=TJm_R2G-K_k

     

    Another thing to consider is that heated plastic degrades very quickly in some cases. Even in a normal injection molding machine some materials (nylon, acetal, delrin) cannot sit inside the barrel for any longer than 30 seconds or so before they start to "burn" or degrade. Also some plastics materials retain moisture (abs, acrilyc) and without being properly dried prior to processing can lead to undesireable molding defects.

     

    Injection Molding is not the only solution to making a plastic part either. There is extrusion molding (pvc piping), blow molding (plastic bottles), compression molding (mostly used for rubber or similiar materials but also plastics in some cases) and combinations of all of these processes with one another and probably even some other processes that I'm unaware of. Vacuum forming is also another widely used method around the modretro and benheck forums which turns out some nice end products.

     

    Again, not trying to rain on anyone parade or tell you that you that it can't be done just trying to be informative. image

     

    Also if you are looking for decent preformed DIY cases for portables or laptops www.polycase.com has a nice selection.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Ashen

    Here's an idea. Got it from youtube. Google home injection molding machines. Looks promising on a small scale.

    http://www.youtube.com/watch?v=Aj6X58ihYqA&NR=1&feature=fvwp