I have two motors and I am trying to attach them to a computer desk. Each of the motors have a separate cord that hook to a power box. It also has a remote to extend and retract the motors. The first motor will raise a platform that my xbox will be mounted on, up through a hole I have made into a door in the top of the desk. The second motor raise a platform in the back of the desk and it will have my 32" tv attached to it. My question that I have is there a way to rewire the base and the remote to operate with the push of a single button to raise both the tv and the xbox instead of raising both individually? Motors originally went to a hospital bed so weight isnt a problem.