• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Veiwer Challenge - Redesigned Wiimote
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 29 subscribers
  • Views 377 views
  • Users 0 members are here
  • hardware
  • mods
  • ps2
  • build_challenge
  • idea
  • viewer_challenge
  • challenge
  • Controllers
  • ben_heck
  • wii
Related

Veiwer Challenge - Redesigned Wiimote

e14 Contributor
e14 Contributor over 15 years ago

As I was playing Monster Hunter Tri on my wii, I noticed that i was holding my wiimote and nunchuck just like i would hold a normal controller. I began craving to play the game game with a true controller, but alas, I didnt have a gamecube controller, nor any money to aquire one, BUT I did did have an extra wii mote and a PS2 controller and it gave me this idea. If you look at the nunchuck, it is simply the left side of a PS2 controller, and the wii mote could be....adjusted to be the right side. wouldit be possible to build one? Later this evening i will add pictures and diagrams to help describe and clarify all of this.

 

Edit: I added the photo. Here is a basic explanation of my badly drawn lines lol :

R1 = C,

R2 = Z,

L1 = 1,

L2 =2,

X = A or B,

Square = A or B,

Start = +,

Select = -,

Analog = Home,

Left analog = Nunchuck Analog,

D-Pad = Wiimote D-pad,

Right Analog stick - Also Wimote D-pad.

 

I also Considered using Triangle as a "trigger" to simulate shaking the nunchuck, and O to simulate shaking the wiimote, if thats possible. Also, the IR sensor would be where the cable originally was, that way you could still point at the screen when needed. Also, have the speaker in the center, between the 1 and 2 buttons

Attachments:
image
  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    I really don't think an idea like this is possible since the board in the wiimote is the same size as the face of the wiimote.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Well, compared to my PS2 controller, the wii mote board was approxamately the same size as the controller horizontally. plus, ben could always make a custom case for it.