element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Viewer Challange: Dual side TV Screen
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 32 subscribers
  • Views 1741 views
  • Users 0 members are here
Related

Viewer Challange: Dual side TV Screen

e14 Contributor
e14 Contributor over 15 years ago

Dear Ben Heck,

     I was thinking maybe if you can make a dual TV for gaming. Me and my brother would play Call of Duty Modern Warfare 2 or Call of Duty Black Ops and we would complain about looking on each others screen when we 1V1 each other on a single TV. I'm pretty sure that people out there don't want to buy a system link cable and get two of the games and two XBoxs, even tho we have two XBoxs we dont have a system link or two of the same game. What I'm thinking is one TV backed up against the other or something like that. I really don't know how to mod so I don't know if this is possible. Well anything is possible when it comes to technology.

 

 

Thanks,

Matthew Harrington

  • Sign in to reply
  • Cancel
Parents
  • RovertScott
    RovertScott over 15 years ago

    I would think that the concept is quite simple and the ability to  combine two screens together wouldn't be too hard, but to achieve the  desired effect may be a bit complicated.

     

    [Possible way to do it]

    You  would want two identical Widescreen LCDs with low depth. Then by  releasing the screens and components from their casing, making a housing  that can hold both screens back to back is a fairly simple build.

     

    However,  this is where things may get complicated. Both screens can't share the  same video input as they both would be identical splitscreen images.  What is required is a piece of hardware and/or Software that can split  the incoming signal from the Console and output the top half to one  screen and the bottom half to the other (also scaling both up). For this  reason we use a pair of Widescreen LCDs, this is due to the normal  Square Image being split into two seprate rectangular images. We want  the best fit for these seprate images, and so a Widescreen LCD would be  the best option, with the Video output set to 4:3 Aspect Ratio (See  Image). *

     

    I am no Hacker by any standard and do not  have the knowledge of electronics to achieve this. I am a Conceptual  Artist who is good with design based problem solving, but I hope I have  provided at least some positive feedback that can be used in achieving  your goal.

     

     

     

     

    *  Personallty I prefer an LCD with a 4:3 aspect ratio, as it can provide a  4:3 or 16:9 image without a shadow of doubt. For some inexplicable  reason there is always an aspect ratio problem when dealing with a  Widescreen LCD. It dosent help that the Software and/or hardware was  made for the Aspect Ratio Ignorant, and so the options don't do what you  need them to.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to RovertScott

    thanks roverscott. its true that slapping two tvs together would be way too easy and that they would have the same image, so they would still have the same picture as the other. my one problem when i was thinking today about splitting the screen was actually splitting it. do you (or anybody that reads this) think there is any kind of hardware/software that could split exactly half of a lcd or led tv.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to RovertScott

    thanks roverscott. its true that slapping two tvs together would be way too easy and that they would have the same image, so they would still have the same picture as the other. my one problem when i was thinking today about splitting the screen was actually splitting it. do you (or anybody that reads this) think there is any kind of hardware/software that could split exactly half of a lcd or led tv.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • RovertScott
    RovertScott over 15 years ago in reply to e14 Contributor

    GardenState, this link shows a method of viewing two images at onces using one screen. However, there is no software for this hardware hack to accomplish the disered effect. http://hackaday.com/2010/08/02/hardware-hack-3d-software-still-needed/

     

    Matt, I was thinking that it shouldn't be too hard to make a piece of hardware that could split a progressive scan image and output them to seprate places. It would require a device that runs 2x as fast as the incoming video, inorder to prevent image flickering or lag.

     

    Console Out -> Device In -> Device Out1 & Out2 -> Screen 1 &  2 In

    Progressive scan goes into the device and ouputs it to Screen1, but when it hits scan line X it switches output from out 1 to out 2.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to RovertScott

    thanks dude that sounds helpful