• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Viewer Challenge : Desktop table *** portable case
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 29 subscribers
  • Views 868 views
  • Users 0 members are here
Related

Viewer Challenge : Desktop table *** portable case

e14 Contributor
e14 Contributor over 15 years ago

Hi Ben

 

Some college going students (I'd be counting myself as one of them in a few months) face this issue. They need a powerful computer, and a laptop is just not enough for their needs. If they go for a desktop, the table occupies a lot of precious space and it's difficult to carry it home every vacations.

 

I was thinking about something that provides the functionality of the PS3 Pelican Case you built, with the design being something like your portable workbench.

 

Here's a crude concept I came up with. It's just an idea to start with.

 

image

Of course, this one wouldn't work at all, but provides a starting point. If you do create an episode on this idea, it'd be great if you  could incorporate an ATX motherboard instead of a microATX, since a uATX  reduces the number of PCI/PCI-E slots available to you, among other  things.

 

Thanks for considering.

 

Ankush Jain

 

Message was edited by: Ankush Jain

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    here is something I got today. Its a I7 core sony Vaio with:

     

    16.4 display

    500gigabyte hard drive

    DVD burner

    Nvidia Geforce GT310M 512 MB Graphics card

    Geunine Windows 7 64-bit

    One year limited warranty

     

    regularly priced 949.99

     

    but for this week only you use coupon code ONP19174 and they bring the price down to 899.99.

    hwere is the webpage.

     

    Sony Vaio

     

    if you want the black version use code RNH19705

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thanks a lot, but there are a couple of problems.

     

    1) 310M is just not good enough for me. If I were to get a lappy, I'd need at least 460M. Even that has problems (prices are 10%-40% higher in my country).

    2) I don't live in US

    3) I can't buy one right now. The only way I get one is if I make it to a 'MIT-like' college, as a gift from my parents, which means, at least 2-3 months from now. imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    I too, am looking at doing a Desktop PC in a Travel Case. The Design i was thinking was to build the Computer piece by piece inside the "base" of the case, with the speakers next to the circuitry. (facing upwards). Then add a wooden "shelf" above the Motherboard and other parts, that had straps that hold the keyboard and mouse in place when the case is closed, but allowed the two to be lifted out without disconnecting them. (as well as holes for the speakers to "speak" through.) then mount the screen to the "top" section of the case, with custom moaning arms (like what ben heck used in the Laptop for frequent flyers episode. The overall idea for mine would be that your computer rests in an easy to carry case when not in use, but can open up and have the keyboard and mouse extend out onto a table, while the Monitor swings down and causes the case to form a triangle shape, Thus allowing it to travel, though it wouldn't have the portablity options of a regular laptop.

     

    You would easily be able to get all the parts for less than an equilavent laptop (Being that you can build a decent custom Computer for around 300-500USD, or get the same specs in a laptop for 500-1000USD (May vary depending on where you buy computer parts, where you live, if you buy a fully assembled computer vs buying each part individually...etc..etc)

     

    Something optional you could add to my rough design would be a flat wooden board resting on 3 pairs of moaning arms that allows it to lift up, over the side of the case, and down. So you'd be able to adjust the height of the mouse and keyboard to your needs.

     

    Just some ideas:

    1)By placing the Monitor on arms it could be moved about and angled to fit your preferences.

    2)Same with the Keyboard/Mouse Shelf concept. Placing them on 3 pairs of arms would allow them to lift up, over and back down to move the mouse and keyboard out of the case without losing an area to use the mouse/keyboard on.

    3) Building the computer part by part is significantly cheaper than buying a stock already made computer/laptop, and it allows you to know exactly what specs you're computer will have.

    4) by making the shelf above the CPU's primary parts you allow yourself the needed ability to replace individual parts without having to disassemble the entire system. (Example: replacing the intial 4 sticks of 512mb ram (sum total of 2gb) with 4 sticks of 1gb ram (for a total of 4) (these are examples i myself use no less than 4gb for any computers i build) )

    5) Placing the speakers in the bottom verses the top allows more room for a bigger monitor. (i believe ben heck used a 21.5 inch screen.)

    and as Mr. Heck always says :"Build it so it can be Taken Part."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thanks for sharing your idea. Since I was gonna be a first time modder, I had decided to do it in a suitcase, since my idea (what I posted at the top) was gonna require more skills. A crude sketch I made :-

     

    http://twitpic.com/3zx5u9

     

    Here's the bummer. Power supply in my country is erratic. While I've got backup power and everything at home, but in college, I doubt there'll be something like this. A UPS for a gaming system I intend to build (i5 2500K, HD6870) would be very heavy, take up a lot of critical budget, hinder(if not kill) portability, and take precious floor space in a college room.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thanks for sharing your idea. Since I was gonna be a first time modder, I had decided to do it in a suitcase, since my idea (what I posted at the top) was gonna require more skills. A crude sketch I made :-

     

    http://twitpic.com/3zx5u9

     

    Here's the bummer. Power supply in my country is erratic. While I've got backup power and everything at home, but in college, I doubt there'll be something like this. A UPS for a gaming system I intend to build (i5 2500K, HD6870) would be very heavy, take up a lot of critical budget, hinder(if not kill) portability, and take precious floor space in a college room.