I have a Mega Super Joy III of Justice or whatever they are and a 2.5" lcd. I've been messing with this build for a while. I've successfully got the game console and the TV powered from 4 AA batteries, but I've been running into some issues. At this point, I would really like to send all my parts to Ben and have him compete this build for me or do one on his own and show it off. I'm not sure what the legal standing is on him doing mods to these pirate clone game systems, but I would really like to see this build. Some things that I would like.
1) Have the original power switch work.
2) Use the original gameboy controls
3) Working original speaker and headphone jack
4) Original power led
5) Contrast potentiometer modified to change between onboard games and external games (make it a switch instead, or just put a switch where it used to be)
6) A modified gameboy game that acts as an adapter for NES games
7) Powered by 4 AA batteries in the original location
I think that's about it. I have all of the parts, but in various states of disrepair. I have a new Mega Super Joy III of Justice in box, and I could get another 2.5" lcd and donate a worthy Gameboy. I would really like to see this done, if for no other reason than for me to be able to follow the tutorial and do it myself.
Another cool thing might be to change the backlight on the lcd to an led backlight and use the contrast pot. to adjust the brightness. In any case I would love to see this episode.