• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Build Challenge --- Super-Computer
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 29 subscribers
  • Views 695 views
  • Users 0 members are here
Related

Build Challenge --- Super-Computer

e14 Contributor
e14 Contributor over 15 years ago

Super computers have been around for a long time.  But unless you've got a couple million dollars in your pocket, you're SOL (Simply Out of Luck). 

 

 

Or are you?

 

 

A recent trend in super computing is to link multiple, off-the-shelf computers into a cluster and use free software to pool all available resources and make it act as one big computer. Of course, they usually come out looking like a lexan delivery truck that got into a wreck with a motherboard delivery van.  But for the researcher on a budget, it's the cheapest way to go.

 

 

The Challenge:

 

 

To design a sleek looking setup that can fit on your desk without taking up the whole surface using a router.

 

 

There is one caveat; Gigabit ethernet is slow.

 

 

I know, I know; it's the greatest thing since sliced bread.  1000 bits a second, it slices, it dices, and leaves the competition in the dust.  To think of improving on the perfection that is this technological Eigth Wonder of the World is MADNESS!

 

 

But there is something better; USB 3.0.  It has a max capacity of 5 GB/s before overhead, and 3.4 after over head.  It costs much less than gigabit ethernet cables.   And I believe if you could combine the MAC addressing system of gigabit ethernet with the bandwidth of USB 3.0 and engineer a USB Router-Switch to link up multiple motherboards, then the end-result would be a 3.4 times faster than ethernet, maybe more because you might be able to decrease the overhead that the USB 3.0 bridge would need to run multiple devices.  What this means is that one motherboard could talk to another, sharing information at transfer rates that are as high if not higher than components on an individual motherboard could (such as the bus that handles CPU and RAM transfers).  Which would translate to more FLOPS a second.  Which would mean more bang for the buck on a researchers already anorexic budget. Not only that, but a device like this could potentially take the place of gigabit ethernet routers in the home.

 

 

There are a couple small-form factor motherboards on the market incorporating USB 3.0 into them, and as the demand for USB 3.0 increases, more are bound to hit the market.  There is a site or two dedicated to the building of small-scale super-computer clusters, and if you want information regarding this build, feel free to contact me.  A great way to increase the flexibility of this system is by dispensing with simple "hubs" that can run fewer than 3 devices at once and convert them into full-fledged switches.

 

That is my build challenge, Mr. Heck;  design a MAC addressing system for a USB 3.0 hub, plug it into an incredibly compact multi-motherboard super-computing, Crysis playing network cluster, complete with all the fancy doo-dads, knick-knacks, and thing-a-ma-bobs that make computers awesome.  It requires more knowledge than the lowly intro-level engineering student that I am possesses to accomplish, or otherwise, we would be having a very different discussion in a forum labeled "Show off your build."  I think that this build, should you choose to accept it, could fill a vital role in the market, both the niche market of super-computer cluster building as well as the commercial one of home-router systems and make USB an even more useful technology than it already is.

 

 

And maybe, just maybe, my children would grow up in a world where they could play Crysis on max settings for under $1200.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    1. Why design a supercomputer to play a game that with a few tweaks and the right video card set up can be playered on most present computers? Thats like using a supernova to swat a fly.

     

    2. Many companies now sell Personal supercomputers. Prices are high, in around 70K, but they are avaible.

     

    3. when suggesting a idea, please consider price, Ben is not made out of money.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    1. Why design a supercomputer to play a game that with a few tweaks and the right video card set up can be playered on most present computers? Thats like using a supernova to swat a fly.

     

    2. Many companies now sell Personal supercomputers. Prices are high, in around 70K, but they are avaible.

     

    3. when suggesting a idea, please consider price, Ben is not made out of money.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Your concerns are duly noted.

     

    1.  The original purpose as stated in my original post is as follows. . . "Which would translate to more FLOPS a second.  Which would mean more bang for the buck on a researchers already anorexic budget.  Not only that but a device like this could potentially take the place of gigabit ethernet routers in the home." The critical element isn't so much the cluster, although, as I said $1250 bucks, while outside his $500 maximum spending limit (how often do projects stay within budget anyway?) is still a feasible project price-tag (if one was trying to make the USB 3.0/cluster combo their goal for this project); however, to focus solely on the USB 3.0 system, as the ONLY device needing inventing within this configuration, was my aim.  A facetious aside comment at the end of a much larger article hardly represents the fundamental aim inherent within the vast majority of the rest of my article.  I understand the dilemma as my post did tends towards ambiguity, and I apologize if my true motive was not readily apparent.

     

    2. and 3.  My idea was originally intended as a viable replacement and upgrade for off-the-shelf gigabit ethernet routers put into what are known as Microwulf Clusters.  Researchers with a limited budget (not withstanding the millions in the consumer market currently using gigabit routers in home networks for a variety of reasons, not just home entertainment) who didn't feel like renting processing time on a larger super-computer, or purchasing that $70,000 dollar supercomputer you mention.  Researchers, like Ben, are also not made out of money, and this project, focussing solely on the USB 3.0 technology which does not exist as opposed to building a micro-super computer cluster which *does* exist is indeed well within his price-range (USB 3.0 hubs run about $30; adding in costs of the low-level programming that would go into this device, my estimate would put it at 120$, as previously stated in my 2nd post); the price-tag for the cluster was merely to illustrate the difference in price-range between professionaly made super-computers and their home-grown equivalents, reinforced here by comparing it to a $70K model.  He also mentions that his goal is to "help out" people who are in need, which it is my contention that such a device as I have suggested would.  Again, my apologies for not making this more distinct as a concept within my first two posts.

     

    I hope I have addressed all of your concerns.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    You know... the more I think about it the more this sounds better and better... but I don't think it can be a simple mod... I think this is a type of re-engineering. I seriously cannot wait to see an optical computer and light peak technology... I myself am trying hard to learn C++ (I am only in my first semester) but I really hope to be a part of a team to bring the next coolest thing to the market. I do have a great Idea... the first "box prototype" will be made of wood similar to those old modems for teletype systems.

    If somehow we could trick USB 3.0 to communicate fro...

    Wait...

    SATA drives (mine at least) only support 3 GB per second. So... if USB 3.0 communicates at 3.5 GB per second this means that SATA 3 at 6 GB per second is overkill "which is better" BUT... what interrupted my thought is BUFFERS, you see, Data usually travels faster via light or bus than it can be saved on a hard disk which is why the HDD have built in cache.. So... a cluster of cheap systems networked via USB 3.0 would not be efficent enough to process data and save it to HD the parts you would need are... Motherboard supporting Intel’s new "Sandy Bridge" 6 core processors, USB 3.0 and at minimum SATA 2.0... But not just one of these systems... they have to be a cluster of them... because this is a supercomputing project... and last but not least... a solid state hard drive which.. According to Computerworld "the OCZ had a read time of 244MB/sec and a write time of 172MB/sec. The Seagate HDD had an average read rate of 98MB/sec and a write time of 87MB/sec." therefore even if we could somehow manage USB 3.0 cluster network on say 10 full power state of the art desktops the HDD can only transfer data at a MAX of 244MB a sec read and 172 MB a sec write.. So for now at least a 1000MB per second network cluster will do everything faster than it can actually save it.

     

    HOWEVER, If and I do mean IF. If we can create software to load massive amounts of data on many many GB of RAM on state of the art memory modules running at 2000 MHZ "DDR3" and not use the hard drives for storage until AFTER all the data has been Processor crunched then perhaps USB 3.0 networking is worth the time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    You are correct, killerfishmonkey, this would be a type of re-engineering.  I was semi-hoping to adapt commercially available programs to my purpose that are already performing a similar purpose in gigabit ethernet. 

     

    As for SATA being better, I looked into it a while back; while its transfer rate is better, Dev's have kept SATA to itself, as any of the sites that I've looked into say it cannot be used for networking computers together.  The only other technology that seems to come close, other than ethernet would be firewire.  However, firewire, while it could've exploded into something as big as USB, sadly didn't, and remains in its own niche as a technology that communicates with media equipment.

     

    In reference to writing to hard-drives, one of the systems in that clustermonkey website uses only one HDD amongst four separate nodes.  I think this somewhat eliminates pitfalls when attempting to recall information because, as I understand it, the program installed on the "head node" will delegate specific portions of a program to the slave nodes, let them crunch it, and then call the information back using the RAM address, saving all of it to it's own RAM allotment (which leads me to believe that the head node should be an ungodly RAM-hog so it can overcome the pitfalls of any system designed with HDD's or SSD's on SATA) without the slave node having to save anything to a HDD.  Once back in the head node, the program inputs the values from the slave nodes into the "master program" if you will, which is then written to the HDD.  Cache's, from what I know of their use, are designed to hold values that are most frequently called; I would think (though don't quote me) that PVM or MPI would be able to allocate the onboard cache memory of each mother board so that, whatever segment of the program each slave node gets would have in its own cache system the values that would normally be called relevant to its own section of the program it was called to run. 

     

    Although, to be honest, I truly and sincerely agree that SSD's are the wave of the future, and some of the cluster layouts in that clustermonkey website do actually call for a small SSD drive for uploading the operating system and other essential programs, then using a larger HDD for the rest.  Of course, as SSD's take off, hopefully we'll be seeing faster transfer rates.  However, I've been noticing in your posts that you seem to be interchanging MB/sec and Mb/sec to mean megabytes a second; the difference, while minute, is crucial, as it is not what I have been referring to in my posts, which is megabits/sec; it takes (usually) 8 bits to make one byte.  So, multiply the read and write speeds times 8, and you will have it's rough read / write time in mega (or giga) bits.  In looking back in my own posts, I have not kept up with the convention myself for writing Gbit/sec or Gb/sec vs. GB/sec.  My apologies, that was misleading of me.  The solid state drives near the top end of the spectrum advertise a read speed 355 MB/sec x 8 =  2 . 840 Gbit/sec which means this will *still* be our bottleneck---but maybe not for long, and it is still close enough to make a lot out of our system, and perhaps enable us to save more money by using even cheaper processors!  The same SSD advertises a 75 MB/sec write speed, so 75 x 8 = 600 Mb/sec.  Or take 3,600 Mb/s for USB 3.0 and divide by 8 which = 450 MB/s, which for some SSD's at about $600 would maintain that holy trinity of RAM - CPU - BUS speeds.

     

    Now, using one that plugs into the PCI-E slot like http://www.ocztechnology.com/ocz-z-drive-r3-p84-pci-express-ssd.html this one advertises 1000 MB/sec read and 970 (sustained 900) write speeds meaning 8 Gb/sec and 7.2 Gb/sec respectively.  Which means an SSD like this which uses the bus speeds of the PCI-E (which is loooooads faster, especially used in conjunction with these particular SSD's, as we can plainly see) would actually take an even faster network, not slower.  This appears to be the top of the line at OCZ, and the slower read / write speeds of the Revodrives mean they are probably cheaper, but all of these SSD's are probably wayyyy outside the price range of the average consumer, or the average small-time researcher, as the case may be.  Again, hoping that demand fuels the need to drive down prices in the future, these will probably be the best options for our information storing needs, and maybe if we only buy ONE uber-expensive component, this particular system arrangement, with a $600 SSD drive will still be cheaper than the "ready-made" computer cluster/bladed systems.  Maybe like the one Maximum PC tested here http://www.maximumpc.com/tags/revodrive .

     

    And yes, SATA 3 would be ideal for the HDD's that are currently wallet-friendly, and while any i Core processor incorporating sandy bridge into it (hopefully without the Cougar Point flaw) would produce eye-popping results, cheap, dual-core processors that the initial super-computing layout call for (bad read/write speeds included) produced tremendous benchmark results, performing at an astounding peak of 26.25 GFLOPS actually maxing out the systems available memory (8 GB's of RAM total; the horror. . .I have 6 on my one desktop alone) before it ran out of raw processing power.  Of course, the head node was built with slightly more robust system components, I think, incorporating a quad core into it as well as being the only motherboard connected to the peripherals and actually being capable of hooking into the internet, as, from what I'm told, a lot of super-computers are not.

     

    killerfishmonkey, I must say it is truly a joy to be discussing this idea with you.  You keep throwing out other ideas for me to consider, and it's a fun challenge, as it tests what I've learned in all the research time I have put into this idea (which I have since lost track of).  I hope I have begun to persuade you of the viability of my idea, if for no other reason than to have someone else to shoot the breeze about it with.  And, I think my own super-computer cluster would be freakin' cool!  But that's beside the point.  I myself am a budding computer programmer (C# for me though, and getting into XNA programming) and I wish you the best of luck!

     

    ***IF MY ORIGINAL INTENDED AUDIENCE (Ben Heck) IS STILL READING THIS, I DO NOT INTEND FOR YOU TO SOFTWARE HACK ANYTHING: MPI AND PVM ARE OPEN SOURCE PROJECTS, WHICH I THINK MEANS THEY ARE *MEANT* TO BE MODDED!!!  THE USB 3.0 HUB CAN BE PROGRAMMED / MODDED USING FPGA's (FIeld Programmable Gate Array's) WHICH MEANS IT'S POSSIBLE NOT TO SOFTWARE-HACK THEM EITHER***

     

    Forgive me System Admin, for I have committed the original sin of typing in all caps for dramatic effect. --- Say Five "Hail Hewlett-Packards" and all will be forgiven, my son.