• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Project Idea - Self-Orienting Antenna
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 31 subscribers
  • Views 858 views
  • Users 0 members are here
  • idea
Related

Project Idea - Self-Orienting Antenna

nbuuck
nbuuck over 15 years ago

This is an idea that I'm hoping to pursue. The goal is to build a chassis that hosts a self-orienting amateur radio antenna (the application of the antenna is not critical). Some of the requirements I'm designing to meet:

 

  1. In this case, the chassis must adjust to fit a 2008 Subaru Forester's cargo racks (not terribly relevant to this site, but a requirement none-the-less).
  2. The system will receive input from a NMEA-compliant GPS receiver.
  3. The system will receive the GPS coordinates of the target transmitter (likely a repeater, but any amateur station).
  4. The system will orient the antenna on the horizontal axis exclusively.

 

Design considerations:

 

  1. An approximately-square board will serve as the base for many of the functional components of the system.
  2. On the top side of the base board, a pinion wheel will host the mount for the antenna.
  3. An adjacent pinion wheel will interlock with the antenna wheel.
  4. The axis of the second pinion will be driven by a motor on the underside of the board.
  5. The motor will be controlled via an onboard FPGA (some brief research shows that the Arduino may be an appropriate solution).
  6. An NMEA GPS receiver with an onboard antenna will be mounted clear of the radio antenna on the topside of the vehicle.
  7. A four line connection from the GPS receiver will connect it to TTL inputs on the FPGA.
  8. The FPGA will calculate the optimal orientation of the antenna by calculating the angle between the orientation of the receiver and the coordinates of the target station.
  9. The target station will likely be specified through some form of practical manual inputs; not sure what the best way to approach this is.
  10. Like Ben's recent vehicle-mounted camera controller project, the system will need to zero out the orientation of the antenna on initialization.
  11. Some form of learning on the part of the program may be required in order to determine direction of travel before orienting the antenna.

 

I just figured I'd share this project since TBHS has been the primary inspiration for the project. Maybe some of you have some ideas about how to practically input the GPS coordinates that the antenna should orient itself toward?

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago in reply to nbuuck +1
    Why not just use 4 antennas and have one in North East South West and have them tethered.
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Have you considered having the controller run the antenna though a (scan) rotation derived from the gps whilst logging the signal/noise. and using the result to align the antenna in the best direction…
  • DAB
    DAB over 15 years ago in reply to e14 Contributor +1
    I thought of the same approach. It ties up less RF hardware than going with the four antennae approach. The key to making it work would be to have a solid signal on during your scan time so you could get…
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Have you considered having the controller run the antenna though a (scan) rotation derived from the gps whilst logging the signal/noise. and using the result to align the antenna in the best direction? Once locked in, directional data from the gps could make adjustments to the rotation, keeping it pointed in the right direction.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 15 years ago in reply to e14 Contributor

    I thought of the same approach.  It ties up less RF hardware than going with the four antennae approach.  The key to making it work would be to have a solid signal on during your scan time so you could get the bearing on the strongest signal.

    The Germans used this approach with a manual scan to find hidden resistance transmitters all over Europe duing the Second World War.

     

    You might be able to get a faster lock on time with a two antenna system on a rotating wheel, because the two signals will enable you to get a good bearing to the signal source with only a 180 degree scan, but again, it uses more RF hardware.  Still, the two antenna approach would also help you quickly determine which direction the source changes from your current position and be much faster at keeping you locked on the source.  That immediate deviation measurement might make it worth going the two antenna route.  With a single antenna, you would have to spend more time scanning to see which direction the source changed.  That problem could force you to go through some rather complex search and track software.

     

    Just a thought.

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 15 years ago in reply to e14 Contributor

    I thought of the same approach.  It ties up less RF hardware than going with the four antennae approach.  The key to making it work would be to have a solid signal on during your scan time so you could get the bearing on the strongest signal.

    The Germans used this approach with a manual scan to find hidden resistance transmitters all over Europe duing the Second World War.

     

    You might be able to get a faster lock on time with a two antenna system on a rotating wheel, because the two signals will enable you to get a good bearing to the signal source with only a 180 degree scan, but again, it uses more RF hardware.  Still, the two antenna approach would also help you quickly determine which direction the source changes from your current position and be much faster at keeping you locked on the source.  That immediate deviation measurement might make it worth going the two antenna route.  With a single antenna, you would have to spend more time scanning to see which direction the source changed.  That problem could force you to go through some rather complex search and track software.

     

    Just a thought.

    DAB