After getting some help from darkuncle33, I have began to draw up plans for the thinest xbox 360 laptop to date. Hist is under 2 inches and I have the ambition to get it under 1.5 inches. My goal is to get it to 1 inch but I will settle for 1.5 inches. It will require heavy modding and I may not finish for a while due to school, but I will hopefully have it done by november and I plan to sell it when I finish. This will be a 15 inch model making it extremley small. But I need some input: I have the wireing for Jtagin a slim should I jtag a xbox 360 laptop? Also obviously the thinner i go we are going to start losing port so I think i will have 2 USB optical hdmi and external monitor inputs. The hardest part will be the dvd drive as I have no idea what I can shave off of it. The heatsink I can work with or even make my own. If you guys have any sugestions please tell. Finally I will be documenting the entire process via live streams and youtube videos, I will figure that out later though. Thanks for any help!
Notes:
No CNC will be used only the shop tools I have.
I plan to use Aluminum. I thought about acrylic but decided not to as when you dremel it the stuff melts and you do not get clean cuts.
Also tell me what a fair price you would pay as I would want to sell it so I could make another one for myself.
--Price if it is under 1 inch and price it is 1.5 inches.