• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum I am trying to build the thinest 360 laptop ever!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 34 subscribers
  • Views 1059 views
  • Users 0 members are here
Related

I am trying to build the thinest 360 laptop ever!

killarshark33
killarshark33 over 15 years ago

After getting some help from darkuncle33, I have began to draw up plans for the thinest xbox 360 laptop to date.  Hist is under 2 inches and I have the ambition to get it under 1.5 inches.  My goal is to get it to 1 inch but I will settle for 1.5 inches.  It will require heavy modding and I may not finish for a while due to school, but I will hopefully have it done by november and I plan to sell it when I finish.  This will be a 15 inch model making it extremley small.  But I need some input:  I have the wireing for Jtagin a slim should I jtag a xbox 360 laptop?  Also obviously the thinner i go we are going to start losing port so I think i will have 2 USB optical hdmi and external monitor inputs.  The hardest part will be the dvd drive as I have no idea what I can shave off of it.  The heatsink I can work with or even make my own.  If you guys have any sugestions please tell.  Finally I will be documenting the entire process via live streams and youtube videos, I will figure that out later though.  Thanks for any help!

 

Notes:

 

No CNC will be used only the shop tools I have.

I plan to use Aluminum.  I thought about acrylic but decided not to as when you dremel it the stuff melts and you do not get clean cuts.

Also tell me what a fair price you would pay as I would want to sell it so I could make another one for myself. 

    --Price if it is under 1 inch and price it is 1.5 inches.

  • Sign in to reply
  • Cancel
Parents
  • Libery13
    Libery13 over 15 years ago

    I have an idea, you could (if the xbox 360 dvd drive is like the computer drives) disassemble just the metal frame around the drive and you would still have all the components in the plastic housing that you could easily cut a bit more and making it a bit thinner, or you could conplitli disassemble the drive from the housing, glue/bolt the laser mount and make the drive in the pelican xbox 360 laptop, that would be a bit risky BUT it would make it the thinner possivel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Libery13
    Libery13 over 15 years ago

    I have an idea, you could (if the xbox 360 dvd drive is like the computer drives) disassemble just the metal frame around the drive and you would still have all the components in the plastic housing that you could easily cut a bit more and making it a bit thinner, or you could conplitli disassemble the drive from the housing, glue/bolt the laser mount and make the drive in the pelican xbox 360 laptop, that would be a bit risky BUT it would make it the thinner possivel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • killarshark33
    killarshark33 over 15 years ago in reply to Libery13

    Well when you take it apart there is really nothing else to shave off of it that I can see without major and I mean major mods to it.  I guess I will have to just settle for a 2 inch laptiop image