element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum help, Rebuilding a better battery for no-name netbook.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 32 subscribers
  • Views 2436 views
  • Users 0 members are here
Related

help, Rebuilding a better battery for no-name netbook.

rayjai
rayjai over 14 years ago

Hey Ben,

 

I have a no-name netbook that I got a few years ago and the battery life only has 1 hour left. I'm trying to find a replacement battery for it but I can't seem to find it. I have no part number to go by. It would be awesome if you or anyone here could help me rebuild the battery by replacing the cells inside. Maybe you could even make it better!

 

I appreciate any help I can get!

 

Ray

  • Sign in to reply
  • Cancel
Parents
  • rayjai
    rayjai over 14 years ago

    I would do that, but It will cover the air holes on the bottom. The battery is located near the front, under the arm rest area. I plan to ditch the battery housing and just stuff it in the battery compartment. the battery can't be wider than 40mm. 45mm might get in the way with the pcb.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to rayjai

    Sorry guys been on holiday. Must say it nice to see people getting envolved. Rayjai its your project, make more air holes; or ditch the housing; or tape it up or mill a battery box, go nuts its your build mate. To avoid the triggering the cutoff, you can simply use a low current powersupply like a cellphone charger to maintain whilst you work, I've not had a chance to study the datasheet so if someone could confirm? Matching is not so much of an issue in parallel as the (cellphone?) psu will maintain the correct voltage to the smart circuit whilst you cut out the old and solder the new, but it would be advisable that they are not massively different, ~0.5 volts should be okay or ditch the psu idea and get both sets at minium capacity (like the batteries are flat) would be easier.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rayjai
    rayjai over 14 years ago in reply to e14 Contributor

    I know i can go nuts, but I want the laptop still be portable. The sony P (knock off) won't be portable anymore with a huge battery pack under it or on top of it. I just want to know if it's still safe to use the 3650mah batteries.

    Do i solder the phone charger to the battery contacts or to the chip directly? I don't understand... I'm afraid I might desolder the battery wires as I solder in new ones. I am still a newb in soldering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rayjai
    rayjai over 14 years ago in reply to rayjai

    Can someone tell me if it's safe to use the 3650mah batteries, when  the battery label says 3800mah?

     

    Here's a photo of the laptop. I have no room to fit any other larger cells and the battery is located on the front of the laptop. so if it's raised, it will be awkard for typing.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rayjai
    rayjai over 14 years ago in reply to rayjai

    Can someone tell me if it's safe to use the 3650mah batteries, when  the battery label says 3800mah?

     

    Here's a photo of the laptop. I have no room to fit any other larger cells and the battery is located on the front of the laptop. so if it's raised, it will be awkard for typing.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rayjai
    rayjai over 14 years ago in reply to rayjai

    Hey guys,

     

    So I bought 6 1700mah batteries and hooked 3 of them up in parallel. So the total mah should be 5100mah right?

    But my battery life is still 1 hour. Did I do something wrong?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • syscorp
    syscorp over 14 years ago in reply to rayjai

    i know little about battery chargers.

    1. chip may have shoutdown - as soon as it detects voltage out of range it will stop working for ever (do not disconnect cells before connecting new ones and use it carefully)

    2. chip may have memory so it does not allow to work longer than it thinks You should - maybe there is battery test option in BIOS (enter during startup)

    3. some batteries may have the possobility to be accessed through software under windows - may test capacity or replace contents of eeprom.

    wanted to do similar thing as You do. finally quit.

    There is also option to use external battery pack with charger and connect instead of power supply - not convinient for sure.

    good luck.