• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum No-No in Schematic shown in Plant Rotation Episode
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 30 subscribers
  • Views 426 views
  • Users 0 members are here
Related

No-No in Schematic shown in Plant Rotation Episode

e14 Contributor
e14 Contributor over 14 years ago

In the schematic shown on the Whiteboard during the episode, Ben shows the N-Channel MOSFET connected as a high-side switch without a high-side FET driver.  Since the AVR and the motor are both referenced to the same ground, the motor will not receive the full supply voltage and the FET will operate in the triode mode causing excessive dissipation.  Better would be to move the N-Channel MOSFET to the low side of the motor (connect source to ground and drain to "-" lead of motor).  This way the MOSFET can be switched into the saturation mode causing much less dissipation and providing nearly full voltage to the motor.  Another option would be to use a high-side FET driver between the AVR and MOSFET.  The last option would be to use a P-Channel FET instead.

 

Granted in the specfic use case of the plant rotater, the MOSFET/motor are not on long enough for dissipation to become an issue.  I just wanted to point it out to others/newbies that may try and adapt the circuit for other uses.

 

Shawn

  • Sign in to reply
  • Cancel
  • colecago
    colecago over 14 years ago

    Yep, I made the same comment on the video.  It becomes even more important if controlling a larger voltage than what your micro supply is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • benheck
    benheck over 14 years ago in reply to colecago

    Thanks for the heads up guys! I'll look into it since I have that plant thing sitting right here.

     

    -Ben