• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Tablet/Laptop hybrid challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 31 subscribers
  • Views 290 views
  • Users 0 members are here
  • android
  • Ubuntu
  • laptop
  • tablet
Related

Tablet/Laptop hybrid challenge

e14 Contributor
e14 Contributor over 13 years ago

This may be way too difficult, but I have an idea for a tablet/laptop hybrid.

 

It seems to me that tablets are going to always be lower powered machines primarily for consuming; however, laptops are used for daily work, so you want them as powerful as possible to produce.  The requirements of the devices prevent them from being converged.  One of the main advantages of having the devices converged is because you never know when you will need some file that is on your laptop while you are on the go.

 

So my idea is to use the base of a laptop running a full OS (preferable Ubuntu), but a tablet can clip into it as a screen.  When the tablet is connected to the base the tablet mounts it as a video out and a storage device, so you can access your files from the laptop, and use the full power of your laptop's CPU (it could even charge the tablet while you are at it).  When the tablet is unclipped, the drive is dismounted and the screen is returned to the tablet's control.  This way you can still access those files, but within the tablets android OS and CPU.

 

Could this be the mobile compromise we need?

  • Sign in to reply
  • Cancel
  • colecago
    colecago over 13 years ago

    I've had this same idea for quite awhile.  If there was a better remote desktop environment out there, or even a standalone remote only OS (like a terminal), that would be awesome.  With how well OnLive supposedly worked, I don't see why there isn't a way to do this on your LAN.

     

    Another option is to use basically a dumb screen/keyboard/mouse combo like this

    http://www.motorola.com/us/consumers/Motorola-Lapdock-100/73945,en_US,pd.html

    And use either long wires for HDMI and USB, or possibly using wireless versions of them (which do exist, not sure the quality or the price).  You could even backpack a pi or another small computer in there and do something like a KVM switch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    you could use a software solution like that alows a pc/laptop to use a tablets screen and mout a network drive. there are many programs that allow you to use a computer as a monitor. maybe make a combination tablet that has a low power computer running the moitor software and a secound that is the power for mobile that releses control to the desktop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • benheck
    benheck over 13 years ago

    I think they already have this, it's called Windows 8 and in stores now!