element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum show idea/challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 30 subscribers
  • Views 253 views
  • Users 0 members are here
  • netbook
  • epic
  • hack
  • project
  • build
  • challenge
  • heck
  • ben
Related

show idea/challenge

e14 Contributor
e14 Contributor over 13 years ago

the challenge is to make a rasperry pi  into a netbook for under $300. you have to have the following:

 

wireless internet (any just as long as you can connect to the internet without any wires or bluetooth)

32 or 64 bit CPU (a good choice would be a intel atom)

A Screen (has to be at least 7 inch)

A GPU (if the CPU doesnt have one already)

fan(s) to keep it cool.

Speakers

Mouse

RAM

HARD DRIVE or at least 32gb USB flash drive

AT LEAST 1 USB PORT (not including if you used  a usb flash drive as hard drive which should be inside the laptop)

ETHERNET

VGA

battery + charger

Headphones jack

Microphone jack

Windows 7 or Linux as operating system.

A keyboard

Power ON and off button

A Case etc to fit it all in

 

This should be possible as long as you buy the cheapest parts.

  • Sign in to reply
  • Cancel
Parents
  • colecago
    colecago over 13 years ago

    Why do you mention the Raspberry Pi and then mention using an atom cpu?  The Raspberry Pi is in itself a computer, you wouldn't need another processor/mobo as well.

     

    As for an Atom based netbook, because of available for purchase components, a homebuilt netbook would never be as good or as cheap as a store bought one.  Manufacturers have parts made for netbooks and small computers and get them made for that purpose.  A homebuilt one would probably end up being a bulky low powered Atom based Laptop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colecago
    colecago over 13 years ago

    Why do you mention the Raspberry Pi and then mention using an atom cpu?  The Raspberry Pi is in itself a computer, you wouldn't need another processor/mobo as well.

     

    As for an Atom based netbook, because of available for purchase components, a homebuilt netbook would never be as good or as cheap as a store bought one.  Manufacturers have parts made for netbooks and small computers and get them made for that purpose.  A homebuilt one would probably end up being a bulky low powered Atom based Laptop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to colecago

    I REALY agree, your very smart colecago