element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Show idea/question? Combined 3d printer, CNC router (& laser cutter?)
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 36 subscribers
  • Views 2539 views
  • Users 0 members are here
  • hardware
  • build
  • build_challenge
  • idea
  • challenge
  • ben_heck
  • show_idea
Related

Show idea/question? Combined 3d printer, CNC router (& laser cutter?)

e14 Contributor
e14 Contributor over 13 years ago

Hello people,

 

There's this idea in my head that keeps popping up:

 

Al these 3d printers, CNC's and laser cutters are (as far as I can tell) for the most part the same hardware.

And the axis and stepper motors do not come cheap.

Wouldn't it be awesome to combine these machines (if possible)?

By perhaps changing the extruder for a dremel/CNC head (or laser)?

 

If it's possible I would call it the Cerberus image (or Two Face in case the laser doesn't work out).

 

If it's not possible I would like to know why, so I can let it rest image

 

Thanks in advance for reading and possibly responding.

  • Sign in to reply
  • Cancel

Top Replies

  • colecago
    colecago over 13 years ago +1
    The only comments I have, is that often CNC machines and 3D printers require different architectures, sure they are both 3D machines, but a 3D printer requires speed and not much torque and can use a lot…
  • ckraft
    ckraft over 13 years ago +1
    This idea comes up quite often. Usually someone attaches a 3D printing extruder to their CNC machine. I warn folks it won't work well but its one of those things you have to do for yourself to believe…
  • ckraft
    ckraft over 13 years ago

    This idea comes up quite often. Usually someone attaches a 3D printing extruder to their CNC machine. I warn folks it won't work well but its one of those things you have to do for yourself to believe. It doesn't work well, which is why you rarely see it. In the case of CNC machines with 3D extruders what you usually find is the person gave up on it because although it worked it ran so slow it took several days to print something you can print on a proper 3D printer in a few hours.

     

    I know these guys are working on a similar idea but I personally doubt the 3D part of it will work well enough. http://www.qu-bd.com/blog/

     

    3D printers need speed. Lots of speed. In order to print something within a reasonable time frame. Even at high speeds it can still take quite a while to print something. I usually print close to 100mm/sec and am building a new printer that will hit around 260mm/s. To achive those speeds you need something that can move that fast. We use a combination of motors + gears + belts to give us the needed speeds.

     

    With a CNC machine you need, as was mentioned above, torque. Cutting requires a lot of torque in order to make a consistent cut. So belts are not found on CNC machines. They are usually direct drive against ACME threaded rod of some kind of ball screw or similar type of highly accurate, high torque drive mechanism.

     

    I could go on. I understand the desire, one machine to meet all your goals. The problem is you would end up with one machine that can do three things not very well, or get three machines that do what they need to do very well. The old saying "Jack of all trades, master of none" does come from somewhere.

     

    As far as Ben doing this in an episode. I don't know. This would be very expensive, the laser tube plus power supply is $1K alone and that's for a cheap Chineese one. Plus Ben really, really, dislikes combo systems. I see him cringe every time he gets a request for combo game systems. I suspect he would feel similarly about this.

     

    -- Chris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to ckraft

    Your point for Ben not wanting to do this is probably right.

    Such a shame but I guess we all want Ben to turn our ideas into cool projects.

     

    So the problem with the printer/CNC combo is that the motors are to slow.

    Isn't there a way to solve this with motors with variable speeds/gearbox? (Sorry if this is a stupid question, somewhat of an electronics n00b).

     

    From the reactions the concensus seems to indeed be pretty well summed up in "Jack of all trades, master of none".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • benheck
    benheck over 13 years ago

    Chris and Coleco are correct. 3D printers and lasers need speed, CNC mills need torque. You can't get both.

     

    I did see a Shopbot at Makerfaire with a 3D printhead on it. Of course it can be done but the question usually is - is it practical?

     

    Also don't feel that we're blowing off the idea, it's just that between myself, Chris and Coleco, we have many years of CNC experience so we've run into this issues time and time again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to benheck

    Thank you for replying.

     

    Using some kind of gearbox would not be a solution to providing more torque during CNC usage and more speed during printing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to benheck

    After an hour or two searching so I don't ask for something already addressed elsewhere, this thread seems to be the closest I can come to MY interest:

     

    In your "portable 3D printer, take two" video you mention in ever-so-brief passing that you used a laser cutter to cut plywood parts for things like the extruder carriage.  Obviously that's how they were cut - BUT --

     

    WHY don't you SHOW OFF THAT TOOL AT WORK?  I'd think you would be PROUD to show it off!!!!  Is it something you built, too, or is it an off-the-shelf purchase?  Don't I want one????

     

    Even the teaser link that offers to let one see/buy parts/tools to "build like Ben" went to a useless, blank page.

     

    So - can you PLEASE shed some light on that handy-dandy tool???

     

    Thanks in advance

     

    jm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • evan.stoddard
    evan.stoddard over 13 years ago in reply to e14 Contributor

    Hey.  I'm not sure what episode it was, it might've been the pocket basic computer episode, but he does show it and talks about it a bit.  It is a commercial one.  Not one he built.  Also in another recent one he talks about how he uses an air compressor to stop flames.  Hope it helps.  Look at some of the more recent episodes.  It must e within the past 10-15 episodes.  Hope this helps!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to evan.stoddard

    Hello Evan

     

    Thanks for your prompt RE -

    but where I FINALLY found reference, and a very BRIEF sighting, was in Ep 3.  Turns out it's a Universal Laser Systems X660, which apparently retails for somewhere in the $35,000 neighborhood.  I'm guessing it's high time that I hosted my own show with sponsors that generous.  Problem with that theory - I don't think I have the charming personality for it.  Surely there's a cheaper way to lase, but at least NOW I KNOW, so I can quit WONDERING.

     

    Thanks again

     

    jm

     

     

     

     

    From: evan.stoddard

    Sent: Wednesday, January 02, 2013 10:57 AM

    To: Jay Murphy

    Subject: - Re: Show idea/question? Combined 3d printer, CNC router (& laser cutter?)

     

     

                

     

          Re: Show idea/question? Combined 3d printer, CNC router (& laser cutter?)

          created by Evan Stoddard in The Ben Heck Show - View the full discussion

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • evan.stoddard
    evan.stoddard over 13 years ago in reply to e14 Contributor

    Don't be so blue yet because you can build one yourself.  Watch a couple more tuts on building a 3d printer and then make a laser with a blueray laser diode and a driver.  You can get those for around 40 bucks online.  Then just build a cnc machine with the tutorials.  It will probably cost you 1500-2000 dollars and it won't be able to cut wood right away but you could probably do a lot of passes.  If not then you can put patterns in wood or cut designs or templates out of paper.  Still a fun project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colecago
    colecago over 13 years ago in reply to e14 Contributor

    And look at this website, lots of homemade laser cutters and CNC machines.

    http://buildlog.net/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to colecago

    Hi all.

     

    I registered to post in this thread.

    I have a 100W CO2 commercial laser that's seeing less work than needed at the moment.

    I have always been interested in 3D printers and even had a guy ask me to cut him a RepRap on my machine some time last year.

     

    Anyway, I have often wondered what it would take to add a 3D printing capability to my machine.

    The hardware is very simple and probably most of you guys are already familiar with it.

    I'll explain in some detail.

     

    The machine has a 1200mm X 800mm workbed.

    X, Y and Z axis move independently.

    They all use stepper motors.

    Each axis has it's own stepper motor driver, X any Y being of the same wattage, Z being significantly more powerful because of the lifting capacity needed.

    The axis are individually controlled by a DSP card.

    The laser is also controlled by the DSP card.

    The laser power can be set by PWM signal.

     

    My initial thought would be to replace the DSP control card by another type of card that can control the Z-axis movement at the same time as the X and Y axis are moving.

    At the moment, Z-axis is only controlled to focus the laser on the workpiece before the job starts.

     

    If such a control card exists, I would be very interested to know about it, be it a DIY solution or a commercially available offering.

     

    Another crude posibility that I thought about would be to somewhat get the machine to output a signal at the end of each layer and this signal would trigger the movement of the Z-axis and adiition of a new layer of material.

     

    Any thoughts/input would be much appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>