• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Show idea/question? Combined 3d printer, CNC router (& laser cutter?)
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 36 subscribers
  • Views 2574 views
  • Users 0 members are here
  • hardware
  • build
  • build_challenge
  • idea
  • challenge
  • ben_heck
  • show_idea
Related

Show idea/question? Combined 3d printer, CNC router (& laser cutter?)

e14 Contributor
e14 Contributor over 13 years ago

Hello people,

 

There's this idea in my head that keeps popping up:

 

Al these 3d printers, CNC's and laser cutters are (as far as I can tell) for the most part the same hardware.

And the axis and stepper motors do not come cheap.

Wouldn't it be awesome to combine these machines (if possible)?

By perhaps changing the extruder for a dremel/CNC head (or laser)?

 

If it's possible I would call it the Cerberus image (or Two Face in case the laser doesn't work out).

 

If it's not possible I would like to know why, so I can let it rest image

 

Thanks in advance for reading and possibly responding.

  • Sign in to reply
  • Cancel

Top Replies

  • colecago
    colecago over 13 years ago +1
    The only comments I have, is that often CNC machines and 3D printers require different architectures, sure they are both 3D machines, but a 3D printer requires speed and not much torque and can use a lot…
  • ckraft
    ckraft over 13 years ago +1
    This idea comes up quite often. Usually someone attaches a 3D printing extruder to their CNC machine. I warn folks it won't work well but its one of those things you have to do for yourself to believe…
  • evan.stoddard
    evan.stoddard over 13 years ago

    I'd buy it!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lean04
    lean04 over 13 years ago

    i´d been thinking about this lately (i didnt come up with those names, they are cool though. I "Quimera" could be a good name also..).

    It would be great if ben could make a diy laser (for a laser cutter) tutorial, since all the material i found on the web are barely paper burning lasers..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colecago
    colecago over 13 years ago

    The only comments I have, is that often CNC machines and 3D printers require different architectures, sure they are both 3D machines, but a 3D printer requires speed and not much torque and can use a lot less durable materials in their design.  CNC machines require stronger bases, steppers configured to run slower and more accurate while providing more torque.  Your axis have to be set up to withstand more weight and have less play because of the forces invovled with a heavy cutting/milling head and cutting into hard materials.  So you can design a CNC machine to be a 3D printer, but its probably not going to be the most efficient 3D printer and probably quite over-engineered.

     

    A 3D printer and laser cutter would at first seem to be a better fit, but you also have to worry about enclosing the whole thing for laser safety, fume extraction and etc, so each machine kind of has their own designs for their own reasons.

     

    I recommend checking out http://buildlog.net/ , they have a good mix of laser/cnc/printers.  In fact, I believe the owner/runner of buildlog is the one who started Makerslide, and also sold 3D printers based on it (ORD bots).  My hobby mill I have is also based on Makerslide.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to colecago

    First off, thank you for your replies.

    colecago, the over engineered part of the 3d printer comes with the fact that you will have one less machine standing in the way and one less machine to buy.

     

    If the sacrifice would be speed, than it probably depends on how much speed you would lose to consider if it's a fair trade-of.

     

    The laser safety could be a problem, thought I do not know what safety measures are required.

    Buildlog sure has loads of projects and makerslide look awesome, thanks for the tips.

     

    I sure would like to hear Ben's opinion about this.

    To me it sounds like the sort of thing he could do.

    Though I was a little bit disappointed he didn't build his own CNC, I would love to have seen that/those episode(s).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lean04
    lean04 over 13 years ago in reply to e14 Contributor

    hi, actually Ben built a CNC machine in one of the first episodes and he shows how he assembles the one in his shop in an episode in which he answers questions and shows his shop around..

    Colecago´s insight looks pretty solid, i don´t have one (yet) but 3d printers seems really slow, and to sacrifice an already slow speed could be too much for me.

    I´d go for a 3d printer/laser cutter, maybe this new year i can start with something.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to lean04

    As I recall it, the CNC he build was more or less just assembling according to instructions.

    The show didn't really suit the time needed for a big project like that, maybe with the increase in episodes this season a long project (like this image) could be done.

     

    After Googling a bit to find some info on hybrid CNC/3d printer/laser cutter, I found the sumpod and easymaker (both CNC/3d printer combo's).

    So it appears to be possible for light milling (according to several forum posts about the sumpod).

    And as far as being slow, this youtube video makes the sumpod look pretty fast: https://www.youtube.com/watch?v=ycU8JwEmRTI

     

    So it looks to be possible to combine CNC and 3d printing, then it must also be possible to combine the laser cutter image

    I can't find anything about the thickness and materials the sumpod can mill.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • John_H
    John_H over 13 years ago

    I wouldn't want the cuttings from a CNC milling machine any where near my 3d printer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    For laser engraving/cutting everything has to be enclosed by metal or laser safety glass, and you're going to need a vacuum setup for fumes as well. For the router setup you need stronger, slower (or much more expensive) motors and much stronger framing. You'd also benefit from a vacuum table, so that's at least easy to combine with the laser cutter. If you did all of this, you'd most likely end up with a 3d printer that wasn't capable of that good of a resolution. Overall, you'd get a jack of all trades, but it would suck at all trades too.

     

    Not to mention with all of this, I don't see this being much less than $10,000 and I haven't seen Ben do many overly expensive builds.

     

    That being said, I would totally love one of these.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bad_boy_y
    bad_boy_y over 13 years ago

    I thing the dust of the cnc (when it's work) can affect laser, miror or extruder. It's can be a problem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bad_boy_y

    Having a way to seal off the sensitive part of the laser equipment when not in use would be simple enough. And you would most likely have the extruder and whatnot be detachable pieces that are only in the machine when you use it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>