• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Portable gamer Challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 29 subscribers
  • Views 400 views
  • Users 0 members are here
Related

Portable gamer Challenge

tejaswivarma
tejaswivarma over 13 years ago

Hi ben

              Can you create a portable gamer (Using raspberry Pi) so that i can just charge the device and go playing any where i want.

Using gamepad so that size can be reduced.

                                                                                                                           - Tejaswi varma

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    omg i thought of this to but my idea was joystick kindof thing like the psp and allso good screen with speakers and mic

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    omg i thought of this to but my idea was joystick kindof thing like the psp and allso good screen with speakers and mic

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    This is my baby project.

    Plays many emu's and ports, browses and multi tasks amazingly well, watches youtube or streaming vids.

    A large set of cells keeps the device going for over 7 days over, 6 months of GSM on standby.

     

    Radio's: WiFi, Bluetooth, ANT 2G/3G/4G.

    Display: 320 X 240

    Inputs: Multi Touch, PS3 Controler, hardware keyboard 

    CPU: 844MHz

    GPU: 160MHz

    Ram: 256MB

    Running Android ICS 4.0.2 and Multi boots to Linux Back Track 7

    32GB SD storage

    32GB USB storage.

     

    And yes it even plays quake 3 online at a solid 30 FPS.

    PS1 games even run on her at 150 to 70 fps. "i often enjoy Descent and Diablo"

     

     

    3 port usb hub attached
    3A 5V source added to drive both the X10 MP and any usb devices.

    Can use any USB HID device.

     


    By pressing the mid home button the device allocates the right analog and triggers
    As a fully fledged mouse input device.

    Binding keys are easy and even touch profiles can be used to simulate touch points.

    Browsing the android device with the Dpad and X, O buttons is as near simple as using the PS3 or PSP XMB.

    I built it as a gaming tool but it has far surpassed my expectations.

     

    image

    image

    I did a similar thing a few years ago.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    Ben I need a job, can't you help a guy out?