element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum cheap DIY 3d printers
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 96 replies
  • Subscribers 40 subscribers
  • Views 8800 views
  • Users 0 members are here
  • 3d_printing
Related

cheap DIY 3d printers

e14 Contributor
e14 Contributor over 13 years ago

what would be the absolute cheapest design to make a 3d printer?  could there be a build on this?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to biomedroy +2
    Dear Roy, I'm a mentor for a high school robotics team and as part of our off-season learning projects we are also building a MendelMax 1.5. Yesterday we got most of the electronics installed and ran a…
  • Vlee489
    Vlee489 over 13 years ago +1
    try http://www.solidoodle.com/
  • Nate1616
    Nate1616 over 13 years ago in reply to e14 Contributor +1
    Docdavies Having built numerous 3d printers over the years including the mendelmax 1.5 I would say you should look at a self leveling bed, upgrade your belts if your using t5/ t2.5 to something like the…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    I am new the the site and am having troubles locating  the information I am looking for so I this is not the correct forum, please direct me to the correct one, thanks.

     

    I am looking to build my own DIY 3D printer so I can print guitar bodies so I am looking for design plans with an large print bed or if I could find someone who could assist me in expanding the RepRapPro designs. 

     

    Any help in me search would be appriciated.

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Olaf Diegel has done some amazing work with 3D printed guitar bodies using only the basic Cubify 3D printer, which is fairly limited in total build volume overall. You should be fine using almost any standard 3D printer, although you can find many examples of oversized systems built out from standard parts. Many of the 80/20 extruded aluminum frame designs (MendelMax, RostockMax, etc) can be extended using off the shelf alternatives without too much difficulty from unsupported spans of metal. The current top of the line for total build volume would be Objet's 1000-series PolyJet or VoxelJet's amazing systems that can tractor material along an internal tunnel as more is added at the front, so you could potentially create granular bound objects larger than the printer itself as long as there is a support for the outfeed. But, do not let build volume alone restrict you - you can piece many larger composites together from sliced sub-components, which helps to deal with issues such as build plate levelling and thermal contraction warping that plague larger prints.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Olaf Diegel has done some amazing work with 3D printed guitar bodies using only the basic Cubify 3D printer, which is fairly limited in total build volume overall. You should be fine using almost any standard 3D printer, although you can find many examples of oversized systems built out from standard parts. Many of the 80/20 extruded aluminum frame designs (MendelMax, RostockMax, etc) can be extended using off the shelf alternatives without too much difficulty from unsupported spans of metal. The current top of the line for total build volume would be Objet's 1000-series PolyJet or VoxelJet's amazing systems that can tractor material along an internal tunnel as more is added at the front, so you could potentially create granular bound objects larger than the printer itself as long as there is a support for the outfeed. But, do not let build volume alone restrict you - you can piece many larger composites together from sliced sub-components, which helps to deal with issues such as build plate levelling and thermal contraction warping that plague larger prints.