• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Every Parents Dream! - A Challenge for Ben Heck
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 33 subscribers
  • Views 1384 views
  • Users 0 members are here
Related

Every Parents Dream! - A Challenge for Ben Heck

timryder
timryder over 13 years ago

My name is Tim, I am a Controls Engineer, I design/program develop automation and robotics for a living. I have been following you for only 4 months now but I've watched everything you've made thus far and have LOVED IT!  I didn't go to school to learn Electrical Engineering I just picked up what I've learned on my own and through resources like you guys here at Element 14!  What a phenomenal program.  There are 2 parts to this e-mail.  I have dozens of ideas for devices I'd like to build and but just don't have the raw basic knowledge of the mass plethora of components out there.  I understand the electrical circuits and theories but the practical applications you can use many of the common IC's out there is where I'm lacking.  Like for example, a while ago on a show you mentioned that you had limited I/O available through an Arduino Uno, so to expand your capacity you added a Bit Shift Register IC which expanded your available I/O and you mentioned that you could basically expand it even more by adding more BSR IC's..... HOW!? This is what I'd love to see. A show dedicated to common components used in the electronics design industry and some uses for them.   This would expand my capabilities as a designer MUCH more.

 

Ok so my REAL challenge!

 

I am a father of 2 and 1 on the way.  I've had this idea for years that I just haven't been able to realize and I'd love to challenge you to make it work!

Design and build a device which can be programmed to record and playback IR commands from remote control devices like a TV or cable Box.  Then when called upon by pressing a kid friendly large button, playback those IR commands in order which will Turn On the TV and Cable Box, Change the Channel to a programmed one.  I think it would be necessary to have a key or some sort of button which would be needed in order to record the IR signals from the remote controls and a handy display to be used for programming it. I don't think you've ever done a show that features the use of IR sensors, this would be a neat one I think many people would repeat.

 

The overall idea is to make a device which would allow a small child 2-5 to be able to turn on their tv and watch their shows without a parents help.

 

What do think?

 

-Tim Ryder

  • Sign in to reply
  • Cancel
Parents
  • QuantumAberrant
    QuantumAberrant over 13 years ago

    There are some pretty advanced TV remotes out there [http://www.logitech.com/en-us/universal-remotes]. But I have been disappointed with most of them as they never know if a device is powered 'on'. This makes programming macros difficult. Does one always assume everything is on or off when putting together a macro? If you have to manually turn on many devices with the remove whats the point of the macro? So, If I may, I'd like to propose a "smart powerstrip' that knows how much power is being used per-plug. Then you can know if the device in plug 1 is on or not. The smart powerstrip could communicate this info to your custom remote, letting the remote know if it shold turn something on or not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to QuantumAberrant

    @QuantumAberrant: If you're using an advanced remote like a Logitech Harmony or more than that the Philips Pronto or Marantz's 9000+ series and newer remotes (all touchscreen, dating back to the early 2000s) they do in fact have a way not to tell but to program a remote code. Most TVs actually have 3 power codes they will accept from remotes. "Change State" which is what most remotes used, as well as "Discrete On" and "Discrete Off" codes. When you program a macro into those smart remotes, you use the discrete codes for your items. I used to program them for friends/family (and even got paid by some friends of theirs to code the remotes they had bought, heh), I had my remote/AV stuff set up so I could pick up my remote, it would sense it and light up, then hit "Watch Movie", then a button for the first letter of the movie (I had the system tied into 2 sony DVD changers w/400 discs each) then scroll through/tap the picture on screen of the DVD's cover art. It would dim the lights (X10 system - at the friend's house he also had sliding vertical blinds and it would close those too), turn ON the tv, turn on the head unit/amplifier, turn on the DVD changer (whichever one was needed), switch the A/V system and TV to the right inputs, and on sci-fi movies it would also change the audio output settings on the head unit to a specific EQ setting I prefer. Oh, and it would also zero the volume level on the head unit (again, using a discrete code) and then turn it up a preset amount (30%) so I wouldn't be shocked if it started too loud. So yeah, I'm still leaning toward it being much more probable to build an arduino-based (or similar) DIY smart remote to counter the ridiculous prices of the professional ones. As a side note, I always bought mine used for $200-300, couldn't afford the $1000+ they cost new. Wish I was kidding.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to QuantumAberrant

    @QuantumAberrant: If you're using an advanced remote like a Logitech Harmony or more than that the Philips Pronto or Marantz's 9000+ series and newer remotes (all touchscreen, dating back to the early 2000s) they do in fact have a way not to tell but to program a remote code. Most TVs actually have 3 power codes they will accept from remotes. "Change State" which is what most remotes used, as well as "Discrete On" and "Discrete Off" codes. When you program a macro into those smart remotes, you use the discrete codes for your items. I used to program them for friends/family (and even got paid by some friends of theirs to code the remotes they had bought, heh), I had my remote/AV stuff set up so I could pick up my remote, it would sense it and light up, then hit "Watch Movie", then a button for the first letter of the movie (I had the system tied into 2 sony DVD changers w/400 discs each) then scroll through/tap the picture on screen of the DVD's cover art. It would dim the lights (X10 system - at the friend's house he also had sliding vertical blinds and it would close those too), turn ON the tv, turn on the head unit/amplifier, turn on the DVD changer (whichever one was needed), switch the A/V system and TV to the right inputs, and on sci-fi movies it would also change the audio output settings on the head unit to a specific EQ setting I prefer. Oh, and it would also zero the volume level on the head unit (again, using a discrete code) and then turn it up a preset amount (30%) so I wouldn't be shocked if it started too loud. So yeah, I'm still leaning toward it being much more probable to build an arduino-based (or similar) DIY smart remote to counter the ridiculous prices of the professional ones. As a side note, I always bought mine used for $200-300, couldn't afford the $1000+ they cost new. Wish I was kidding.