• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum My First Build!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 29 subscribers
  • Views 281 views
  • Users 0 members are here
  • pinball_machine
  • hardware
  • build
  • pinball
  • ben_heck
Related

My First Build!

e14 Contributor
e14 Contributor over 13 years ago

     Hello!! I joined up due to Ben's awesomeness and to show off my digital pinball machine (yes, its an emulator and not a true size pinball table but it is fun).  I am using two monitors hooked up to a PC that has a USB controller for the flippers and plunger and two USB speakers (no extra power wart).

  I am running the Future Pinball emulator and the whole system works great together!  In the different pictures (50 meg but only 5 pics?!) (ill upload more later) you can see how I started out by laying the screens down to figure out the overall size and and angles that worked best, I then started screwing parts together and built the lower half of the frame (I wanted to play!) and mounted the PC motherboard on some feet that I then screwed to the base of the cabinet along with the speakers and power supply, I then drilled for the flipper buttons and the other control buttons.  I put a USB wireless card in for connectivity and it allows me to edit the configuration remotely.

  I then topped the playfield and backglass with acrylic (its sold in 18 inch widths so thats what I made the cabinet to fit (so I only had to cut once))  that I painted on the underside with the same paint i used on the cabinet!

  As a prototype / version 1 I think it came out ok...

Attachments:
image
image
image
image
image
  • Sign in to reply
  • Cancel
  • benheck
    benheck over 13 years ago

    Nicely done, and a great way to use older monitors!

     

    Keep it up!

     

    -Ben