Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Ardunio power Water-Methanol injection controller
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 32 subscribers
  • Views 1852 views
  • Users 0 members are here
Related

Ardunio power Water-Methanol injection controller

e14 Contributor
e14 Contributor over 13 years ago

looking to build my own water-methanol injection controller for my car. At 7lbs of boost I want to mist the mixture all the way up to full spray at 22lbs boost. my pump is 12 volts and up to 15 amps at full power. I found out how to do a scaling input to a scaling output. i don't know what arduino board to use. i assume i need to have a variable motor controller or an H bridge of somesort. Any suggestions? i also want the system active only when the outside temperature is 80°F or above. Need an ouput for a LED or display to show me how active the system is pumping.

  • Sign in to reply
  • Cancel
  • colecago
    colecago over 13 years ago

    I'm not sure if you'd need something as complicated as a motor driver or h-bridge as the pump might just need a unidirectional DC signal, meaning you could just use a single high side or low side FET to control it.  You should look how the pump is being controlled currently.  Also, how are you going to get the boost lb information into your Arduino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to colecago

    I have a tube run into current dead controller that came with my AEM 30 3002 kit. I was looking at a pressure sensor to hook to boost tube from intake to send signal to Arduino for boost reference. I am new to Arduinos but I want to learn.The pump is 12 volts as you supply increasing voltage it pumps faster and faster.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sqkybeaver
    sqkybeaver over 13 years ago

    is this to inject directly into the intake, or over an intercooler?

     

    if the pump is brushless a simple current regulator would do the trick.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to sqkybeaver

    The nozzle is in the intake tube right after the inter cooler. The controller that came with the AEM kit died and I am trying to replace it cheaper and better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • TCPMeta
    TCPMeta over 13 years ago in reply to e14 Contributor

    I don't think a Ardunio can handle as a PCM or ECU. There are too many sensors that has to be looked at to control a fuel to air ratio. Last thing you want is to dump in too much fuel into the engine. I would look into a MegaSquit kit. It's a cheaper route and is made for the applications you want/need.