Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum ddr3  memory to usb adapter
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 31 subscribers
  • Views 1857 views
  • Users 0 members are here
  • ddr3
  • usb
  • memory
Related

ddr3  memory to usb adapter

e14 Contributor
e14 Contributor over 13 years ago

Hi. not sure if there a product already in market. they  seem to be all flash type.

the gold is to give a new life to my old laptop that has only  255MB ram and 512kb max upgradable. its a bit slow  linux and virtualbox apliances and hard disk swap partition.

there are people using usb flash  devices  as  swap but they all warn about fast damaging usb devices.

so way not an adapter ddr3 to boost memory on the fly to old computers like laptops, raspberrypi, old 486 computers or maybe even tablets.

maybe also implementing a software that would manage withch programs run on original memory and witch run on usb ddr3 memmory device

 

cheers image

  • Sign in to reply
  • Cancel
Parents
  • jds123
    jds123 over 13 years ago

    As mentioned by Ryan Dowell, it wouldnt be fast, but the fact that RAM is volitile doesnt really matter, because you could probably just have a nand chip with the partition information on it. But it would be difficult to build such a device because RAM is accessed by memory location, and then sends out the data at that location, so you would have to change the signal to communicate through usb (which is basically very fast serial) which would be a difficult task. you're probably better off buying a mechanical external harddrive as they last longer than nand chips and would still provide the memory neccesary.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jds123
    jds123 over 13 years ago

    As mentioned by Ryan Dowell, it wouldnt be fast, but the fact that RAM is volitile doesnt really matter, because you could probably just have a nand chip with the partition information on it. But it would be difficult to build such a device because RAM is accessed by memory location, and then sends out the data at that location, so you would have to change the signal to communicate through usb (which is basically very fast serial) which would be a difficult task. you're probably better off buying a mechanical external harddrive as they last longer than nand chips and would still provide the memory neccesary.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jds123

    External hard drives often come with between 8 and 128MB of RAM serving as a cache.

    http://en.wikipedia.org/wiki/Disk_buffer

    so frequently you would be accessing RAM anyway, even when using a hard drive,

    with the benefit of the hard drive's non-volatile storage.

     

    In general you want to use expensive peripherals with expensive computers,

    and cheap peripherals with cheap computers.  Otherwise the mismatch will

    usually result in wasted capability.