Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Portable Pi Power Problems
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 32 subscribers
  • Views 910 views
  • Users 0 members are here
Related

Portable Pi Power Problems

e14 Contributor
e14 Contributor over 13 years ago

I am working on a portable Raspberry Pi project and am having a bit of trouble finding a power supply that will do what I want it to do. I am looking for something that will step down from 7.4V to the 5V the system will need, as well as allow the system to operate while charging. am I just over complicating things? or is there an off the shelf unit I can build into the system?

  • Sign in to reply
  • Cancel
Parents
  • colecago
    colecago over 13 years ago

    You can indeed use a linear or switching regulator to do this, linear regulators are more wasteful so a switching is preferred, look up Rohm BP5275-50.

     

    Another option is using a single cell, or multiple parallel cells so you boost to 5V, then you can use something like this

    https://www.sparkfun.com/products/11231

     

    Which has the buck/charging circuit for a Lipo and then the boost to 5V all on one board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colecago
    colecago over 13 years ago

    You can indeed use a linear or switching regulator to do this, linear regulators are more wasteful so a switching is preferred, look up Rohm BP5275-50.

     

    Another option is using a single cell, or multiple parallel cells so you boost to 5V, then you can use something like this

    https://www.sparkfun.com/products/11231

     

    Which has the buck/charging circuit for a Lipo and then the boost to 5V all on one board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to colecago

    The first problem I am running into is the Li-Po pack I've found that I think should work is 7.4v which is a bit much for the pi so the first requirement for the power supply is that it steps the voltage down to 5v at least.

     

    I would also like to beable to use everything while its charging, that way I can hook it up to a display and use it as a compute as well, if it can charge while active and plugged in thats great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    i dont know about that but the first one is the one ben used