Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Portable Pi Power Problems
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 32 subscribers
  • Views 910 views
  • Users 0 members are here
Related

Portable Pi Power Problems

e14 Contributor
e14 Contributor over 13 years ago

I am working on a portable Raspberry Pi project and am having a bit of trouble finding a power supply that will do what I want it to do. I am looking for something that will step down from 7.4V to the 5V the system will need, as well as allow the system to operate while charging. am I just over complicating things? or is there an off the shelf unit I can build into the system?

  • Sign in to reply
  • Cancel
Parents
  • colecago
    colecago over 13 years ago

    If you are using the same screen as Ben, we've successfully tied off the 5V line inside of the LCD to power the Pi, and that's how we'll do it on the improved version of the portable.  Just bring the 7.4V into the 12V input on the screen, then tack a wire out of the 5V output and take it to the Pi.

     

    The downside to this setup is that the regulator cuts out about 6.4ish volts, so you are losing capacity there.  With the new Pi with the boost convertor, we should be able to use the batteries down to a lower level definitely increasing the run time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colecago
    colecago over 13 years ago

    If you are using the same screen as Ben, we've successfully tied off the 5V line inside of the LCD to power the Pi, and that's how we'll do it on the improved version of the portable.  Just bring the 7.4V into the 12V input on the screen, then tack a wire out of the 5V output and take it to the Pi.

     

    The downside to this setup is that the regulator cuts out about 6.4ish volts, so you are losing capacity there.  With the new Pi with the boost convertor, we should be able to use the batteries down to a lower level definitely increasing the run time.