Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum NAS Build Idea
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 31 subscribers
  • Views 726 views
  • Users 0 members are here
Related

NAS Build Idea

e14 Contributor
e14 Contributor over 13 years ago

Looking to see if you would do a NAS build using the Rasberry Pi and with hot swap bays that can accept 3.5" and/or 2.5" HDD's. Software could be FreeNAS. Needs to connect with gigabit ethernet to the home network.

  • Sign in to reply
  • Cancel

Top Replies

  • benheck
    benheck over 13 years ago +1
    Personally, I would use an older full-sized PC with Linux for a NAS. Unless there's a reason it needs to be small, not sure why I'd use the Pi.
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    This will be connecting to a gigabit network so might as well have the same on the NAS if possible. If the RPi is too slow and can't connect SATA to have multiple HDD's then something else will have to do. The Fit PC3 looks perfect for size and performance but not for the price in this project. For that price might as well go with a polished system like a Drobo. What I'm looking for ultimately is a NAS that is like the Drobo Mini and the Drobo 5n. If the Drobo Mini had gigabit ethernet it'd be perfect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    This will be connecting to a gigabit network so might as well have the same on the NAS if possible. If the RPi is too slow and can't connect SATA to have multiple HDD's then something else will have to do. The Fit PC3 looks perfect for size and performance but not for the price in this project. For that price might as well go with a polished system like a Drobo. What I'm looking for ultimately is a NAS that is like the Drobo Mini and the Drobo 5n. If the Drobo Mini had gigabit ethernet it'd be perfect.