Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Problems with soldering tips!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 32 subscribers
  • Views 621 views
  • Users 0 members are here
Related

Problems with soldering tips!

toxxn
toxxn over 13 years ago

Recently I got a new soldering iron from radioshack. I have used it on several projects and it has worked very well thus far. The last project I was working on, I noticed a small indentation on the end of the tip. I just got done desoldering some componets moments ago when I noticed the indentation has gotten bigger, looking like a cavity. I am sure most of you will already know exactly what I mean, but here is a couple pictures to illustrate what I am reffering to:

 

image

image

 

I know the pictures are a little fuzzy, though I took them using my iPod.

I am concerned about this tip and I am unaware as to why it has done this espeically since I have only had the iron itself for 4 days and have only used it for a few projects, using up maybe a foot of solder.

Could someone whom is more experienced with soldering irons please give me some info as to what causes this and why? and perhaps some info as to what should be done about it.

I am just going to replace the tip for now,

  • Sign in to reply
  • Cancel

Top Replies

  • gdstew
    gdstew over 13 years ago in reply to johnbeetem +1
    While the wet sponge does work (I used it for many years myself) I much prefer a different type of tip cleaner that uses a ball of fairly wide (about 1/64 inch or ~ 39 cm) metal "fibres" kind of like steel…
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    You have to keep the tip coated with solder, or the tip's iron metal quickly oxidizes and corrodes away.  Adding the solder is called "tinning".  There's some explaination at Wikipedia, and I'm sure others know of links to better resources and tutorials.

     

    Here's what I do: when I first use a tip, I melt solder onto it as it warms up so that it is fully coated.  Tips usually come pre-tinned, but I like adding more solder.  I always have a moist sponge handy to clean excess solder and flux off the tip.  After soldering one or a few joints, I wipe the tip on the moist sponge and then add fresh solder to make sure the tip stays coated.

     

    Once a tip has any iron metal exposed and oxidized, the problem will only get worse.  Solder won't stick to the exposed iron oxide, which makes re-tinning a problem.  There might be tricks for sanding down the oxide so you can re-tin, but I've never tried them.  I usually just keep a spare tip handy and think of them as "consumables".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • toxxn
    toxxn over 13 years ago in reply to johnbeetem

    Thanks for the info John.

    I have tried to keep my tip "tinned" although I guess when I cleaned off my tip with a wet sponged I just carelessly forgot to re-tin it. Lesson learned I supposed.

    You have to fail to succeed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • toxxn
    toxxn over 13 years ago in reply to johnbeetem

    Thanks for the info John.

    I have tried to keep my tip "tinned" although I guess when I cleaned off my tip with a wet sponged I just carelessly forgot to re-tin it. Lesson learned I supposed.

    You have to fail to succeed.