Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Challenge for Ben: Arduino based smartphone
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 32 subscribers
  • Views 994 views
  • Users 0 members are here
Related

Challenge for Ben: Arduino based smartphone

e14 Contributor
e14 Contributor over 12 years ago

A cool challenge I think would be interesting to see Ben attempt is making a small, portable Arduino based smartphone, using this software here https://github.com/yexiaobo-seeedstudio/ArduinoPhone and with similar hardware to this here http://www.instructables.com/id/ArduinoPhone/?ALLSTEPS

 

So what do you guys think?

 

Regards,

Totara / Will

  • Sign in to reply
  • Cancel
Parents
  • yuritikhonov
    yuritikhonov over 12 years ago

    I think full size arduino is not so good for a smartphone. May be arduino pro mini?

    And I would prefer building the device in cyberpunk style, it would be a great alternative to the iPhone image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • yuritikhonov
    yuritikhonov over 12 years ago

    I think full size arduino is not so good for a smartphone. May be arduino pro mini?

    And I would prefer building the device in cyberpunk style, it would be a great alternative to the iPhone image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to yuritikhonov

    i really think you guys are missing the point.  the ATmega328 has a clock speed of 16 MHz, most feature phones have more power than that it's just not the kind of thing that would work well


    You may be able to get away using the Raspberry pi but even that is low power by today's phone standards.  the average phone is 1.5 GHz dual core and the Pi is 700 MHz BUT running an old version of android it would be fine.  the real problem is making it read sim cards correctly!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor


    wow okay the 700mhz is not a lot granted..but average phones have 1.5ghz...are you out of your mind the iphone was just about over 500ghz last time i checked and the Samsung galaxy s3 1ghz Sony experia only 1ghz htc 1 1ghz....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    apple and Samsung haven't made single core phones for over 2 years!!! so you may be able to load android 1.6 on it and have it be stable.  even my 5 year old sony hs a 1gz processor and lags on 2.0

     

    the SGS3 is a 1.4ghz dual core and is a year and a half old

    the SGS4 is a 1.6ghz quad core

    the HTC 1x is 1.5GHz quad core

    the iphone 5 is 1.3ghz dual core and is over a year old (the 5s is the same)

    the sony xperia Z is 1.5ghz quad core

     

    and the big 2

     

    SG note 2 1.6ghz quad core

    SG note 3 2.3ghz Quad core

     

    now if you ignore the notes you get an average of 1.46 ghz and the average amount of cores is 3.2 cores

     

    you also need to keep in mind that all of these phones have large Graphics processors to

     

    NOW.... this is not to say that the RBP can't do it infarct it could but by today standards it wouldn't be considered a smart phone as it would have to run a very old version of android!  it would feel like an iphone 3g or an ipad 1, neet but very little use .

     

     

    HOWEVER i love the idea of building it just to build it but due to the lack of sim dialing compatibility i would make something like a 7" tablet it would be cool cause oyu could also dual boot it with a desktop os like raspbian