element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 3D printing and prosthetics
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 31 subscribers
  • Views 2240 views
  • Users 0 members are here
  • build_challenge
  • idea
  • ben_heck
  • prosthetics
  • show_idea
Related

3D printing and prosthetics

e14 Contributor
e14 Contributor over 12 years ago

If your looking for a hard challenge, then take a look a how to build Body powered or Electronic powered finger prosthetics.  I would think with the ability to do 3D printing, it should not be possible.

 

As a disabled veteran and four finger amputee I have more than a couple challenges in life, and one of the biggest has been what I call work shop prosthetics.  The VA Hospital provided me with prosthetic fingers (a couple grand per finger) but they are for looks only, and because they are silicon they have no support.  what is needed is something a bit more complex, but more heavy duty than the Xfingers on the market, but zero need to look like real fingers.  it's about function and not looks, that provides a bit more dexterity and grip then what we currently have.  something to strap to the wrist so it stays on, and allow the use of holding a tool.  not being able to work with tools much at all has been one of the hardest things to get used to for the last 7 years. originally I was a gunsmith, and intended to teach myself engraving, but holding a small tool in my left hand and a hammer in the right, seems to get in the way. in fact anything as simple as trying to carry a clothes basket, or bags after shopping with the left hand can be troublesome, especially because i have to hold a cane in the right.   for the longest time i tried to build something that I could just slip a glove over that would add length, and the ability to hold something as simple as a can (holding a small tool like a punch would be the ultimate goal in time) but just being able to slip something on and be able to lift or grab tools or everyday items like a fry pan to cook would be the goal.   I'm not talking about bionics or top of the line prosthetic design.  just something for the purpose of working around the house, that's 100% usability and zero % looks is what is needed.  something thats more TOOL than the current line of prosthetics on the market.  that have arms, hands, legs feet, but when it comes to fingers (especially multi fingers) the only thing available is a fake finger for looks and not for use.  and that is what needs to change.  it just needs someone to look outside the box for once.

 

how is that for an extreme challenge

  • Sign in to reply
  • Cancel

Top Replies

  • vsluiter
    vsluiter over 12 years ago +1
    Anyone interested in helping gamers with physical problems: www.thecontrollerproject.com
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Howdy Gary. I have a couple questions.

    Does your thumb work?

    do you have any digits that could signal a grasp?

    Do you have wrist movement?

    Can you cup your hand, as if to put it inside a narrow tube throughout wrist rotation?

    Can you expand your palm flat throughout wrist rotation?

    Will you wear a logo?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    did you have any other options to look into?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I am looking into the "Robofinger".  You can check them out at robohand.net.  One of their representatives contacted me today.  She stated that the cost is $200 per finger plus $300 for the orthoplastic and fitting etc. Robohand has a free open-source download for a 3d printable  full hand prosthesis.  People can print from home, rent a 3d printer, or hire an outside source to print the device.  The pieces click together like Legos.  Unfortunately there is not a 3d printable version for the partial finger amputee, hence your challenge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Robohand's prices are much more affordable than the x-finger and other functional devices. Aquatip prosthesis, http://letcdesign.com/, which allows the user to "feel" with the tip of their prosthesis. The Bio-mechanical prosthetic finger  at http://rcmenterprise.com/ is also functional, but pricey.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Robohand's prices are much more affordable than the x-finger and other functional devices. Aquatip prosthesis, http://letcdesign.com/, which allows the user to "feel" with the tip of their prosthesis. The Bio-mechanical prosthetic finger  at http://rcmenterprise.com/ is also functional, but pricey.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colecago
    colecago over 12 years ago in reply to e14 Contributor

    A tip you can feel, huh?  That's a pretty interesting area.  I've always thought alternative human interfaces and artificial senses were interesting.  I should look more into the prosthetic work people are doing.