element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Great Glue Gun Recap!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 30 subscribers
  • Views 518 views
  • Users 0 members are here
  • gluegun
  • hot_glue
  • ben_heck
  • arduino
Related

Great Glue Gun Recap!

colecago
colecago over 12 years ago

I recently helped out behind the scenes of the two part Ben Heck Great Glue Gun episode. I helped out on the electronics design, assembly, and the firmware.  As he rarely does write ups I thought I’d post the code (pre hall-effect) and the parts I remember using for others to follow in the great glue gun foot steps.

Here is a partial working demo early in the process

https://www.youtube.com/watch?v=g92pjOrOWOE

 

 

Parts (cross referenced the best I could, I used Sparkfun parts unfortunately, so no warranties!)

BenDuino (Ben's custom Arduino Uno, link is similar but larger ->) A000066 - ARDUINO - DEV BRD, ATMEGA328, ARDUINO UNO R3 DIP ED | Newark element14 US

H-Bridge SN754410NE - TEXAS INSTRUMENTS - IC, PERIPHERAL DRIVERS, HALF-H, 36V, 1A, DIP-16 | Newark element14 US

Trigger Pot (retired) https://www.sparkfun.com/products/retired/10314

SSR S202S02F - SHARP - SSR, PC BOARD, 8A, 80VRMS TO 240VRMS | Newark element14 US (We used a different SSR but this is similar)

Proto board wtih ground plane https://www.sparkfun.com/products/8811

Wall Wart 9V WSU090-0800-R - TRIAD MAGNETICS - AC-DC CONV, EXTERNAL PLUG IN, 1 O/P, 7.2W, 9V | Newark element14 US (We used a different wall wart but this is similar)

Thermistor 10k B57891M0103K000 - EPCOS - THERMISTOR, NTC, RADIAL LEADED | Newark element14 US (change the code for a 10k, I ended up ruining my 10k's and falling back on a 100k)

RGB LED L-154A4SUREQBFZGEW - KINGBRIGHT - LED, MULTICOL., RGB 5MM, X-BRIGHT | Newark element14 US  (We used a 10mm not a 5mm)

 

Code

#include <math.h>

#define MotorENPIN  3

#define Motor1APIN  2

#define Motor2APIN  4

#define Light1PIN  5

#define Light2PIN  6

#define minSpeed 50

#define maxSpeedLow   90

#define maxSpeedHigh  160

#define meltTemp 235

#define speedTempOffset 25

//#define SSRPIN    7

#define ThermistorPIN A0                 // Analog Pin 0

#define TriggerPIN  A1

//#define TempSetPIN  A2

boolean extruding = false;

boolean atTemp = false;

int maxSpeed = maxSpeedLow;

int updateCount = 0;

int setTemp = 0;

int reqSpeed = 0;

int setSpeed = 0;

int temp;

int count = 0;

float pad = 100000;                       // balance/pad resistor value, set this to

                                        // the measured resistance of your pad resistor

float thermr = 100000;                   // thermistor nominal resistance

float Thermistor(int RawADC) {          //converts thermistor reading into a resistance and then temperature in C

  long Resistance;

  float logVal;

  float tempTemp;  // Dual-Purpose variable to save space.

  Resistance=((1024 * pad / RawADC) – pad);

  logVal = 3950/log((float)100000/Resistance);

  //T2= T1*B/ln(R1/R2)  /  ( B/ln(R1/R2) – T1 )

  tempTemp = (25+273.15)*logVal;

  tempTemp = tempTemp / (logVal-(25+273.15));

  tempTemp = tempTemp – 273.15;  // Convert Kelvin to Celsius

  tempTemp = (tempTemp * 9.0)/ 5.0 + 32.0;                  // converts to  Fahrenheit

  return tempTemp;              // Return the Temperature

}

void setup() {

  Serial.begin(115200);

  pinMode(MotorENPIN, OUTPUT);

  analogWrite(MotorENPIN, 0);

  pinMode(Motor1APIN, OUTPUT);

  digitalWrite(Motor1APIN, LOW);

  pinMode(Motor2APIN, OUTPUT);

  digitalWrite(Motor2APIN, LOW);

  pinMode(Light1PIN, OUTPUT);

  digitalWrite(Light1PIN, HIGH);

  pinMode(Light2PIN, OUTPUT);

  digitalWrite(Light2PIN, LOW);

  //pinMode(SSRPIN, OUTPUT);

  //digitalWrite(SSRPIN, LOW);

  analogRead(ThermistorPIN);

  analogRead(TriggerPIN);

  //analogRead(TempSetPIN);

}

void loop() {

  int readTemp = Thermistor(analogRead(ThermistorPIN)); // read ADC and  convert it to F

  if ((readTemp > 0) && (readTemp < 500))

    temp = readTemp;

  //setTemp = analogRead(TempSetPIN);

  //setTemp = map(setTemp,0,1023,50,350);            //analog reading 0-1023, temperature range 50 to 350F

  if (temp <= meltTemp){                            //if less than set temp, turn on SSR, set lights

    //digitalWrite(SSRPIN, HIGH);

    digitalWrite(Light1PIN, LOW);

    digitalWrite(Light2PIN, HIGH);

    maxSpeed = maxSpeedLow;

    atTemp = false;

  }

  if ((temp > (meltTemp + 5)) && (temp <= meltTemp + speedTempOffset)){  //if greater than set temp but less than set temp + 10, set lights

    digitalWrite(Light1PIN, HIGH);

    digitalWrite(Light2PIN, HIGH);

    maxSpeed = maxSpeedLow;

    atTemp = true;

  }

  if (temp > (meltTemp + speedTempOffset + 5)){                        //if greater than set temp + 10, turn off SSR, set lights

    //digitalWrite(SSRPIN, LOW);

    digitalWrite(Light2PIN, LOW);

    digitalWrite(Light1PIN, HIGH);

    maxSpeed = maxSpeedHigh;

    atTemp = true;

  }

  reqSpeed = 1023 – analogRead(TriggerPIN);

  if (reqSpeed < 3){                                 //if less than 3 (deadzone) and was extruding, reverse the motor to suck in the gluestick

    if (extruding == true && count >= 450){

      analogWrite(MotorENPIN, 0);

      delay(50);

      digitalWrite(Motor1APIN, LOW);

      digitalWrite(Motor2APIN, HIGH);

      analogWrite(MotorENPIN, 125);

      setSpeed = 0;

      delay(150);

      analogWrite(MotorENPIN, 0);

      delay(50);

      extruding = false;

      count = 0;

    }

    else{                                              //if less than 3 (deadzone) and was not extruding or reverse timed out, turn off motor

      count = 0;

      analogWrite(MotorENPIN, 0);

      setSpeed = 0;

    }

  }

  else if (reqSpeed > 5 && atTemp == true){                              //if greater than 5 (deadzone), turn on motor mapped to stick, 5-1023 reading 50-150 motor, set extruding

    if (count < 450)

      count++;

    setSpeed = map(reqSpeed,5,1023,minSpeed,maxSpeed);

    digitalWrite(Motor1APIN, HIGH);

    digitalWrite(Motor2APIN, LOW);

    analogWrite(MotorENPIN, setSpeed);

    extruding = true;

  }

  if (updateCount <= 250)

    updateCount++;

  else{

    writeUpdates();

    updateCount = 0;

  }

  //writeUpdates();                                      //for debugging

}

void writeUpdates(){

  Serial.print(“Temp: “);

  Serial.print(temp,1);

  Serial.println(“”);

  //Serial.print(“Req Speed: “);

  //Serial.print(reqSpeed,1);

  //Serial.println(“”);

  //Serial.print(“Set Speed: “);

  //Serial.print(setSpeed,1);

  //Serial.println(“”);

}

As always code and parts list offered without warranty and very little support :-)

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    I have been planning a 3d printer hot-blue extruder.

    I am much more interested in what 3d printed parts were used!

     

    Do you have any access to the 3d files, I would like to post them in an open source website like Thingiverse. Allowing the designs to grow and adapt.

     

    I think a lot of the community may appreciate this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colecago
    colecago over 12 years ago in reply to e14 Contributor

    I'll talk to him about this next time I see him.  Its similar to a design he has done with extruders for his 3D printers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colecago
    colecago over 12 years ago in reply to e14 Contributor

    I'll talk to him about this next time I see him.  Its similar to a design he has done with extruders for his 3D printers.