element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum line following robot - do i need 2 motor drives to control 4 motors
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 30 subscribers
  • Views 440 views
  • Users 0 members are here
  • motor_drives
Related

line following robot - do i need 2 motor drives to control 4 motors

e14 Contributor
e14 Contributor over 12 years ago

i'm making a line following robot with 4, 6V dc motors. I'm currently using L293D motor drive. My current idea is to connect two motors with each of the output pins. But i'm afraid this configuration may burn the chip. But in the data sheet, they said each output pins can deliver upto 600 mA. The motors i'm using need 120 mA. Can anyone help me.

  • Sign in to reply
  • Cancel
Parents
  • colecago
    colecago over 12 years ago

    Putting motors in parallel off a single drive doesn't work well.  Motors are pretty dynamic devices and if one stalls it will take all the current from the other one in parallel causing weird behavior.  Why are you using 4 motors instead of 2 anyways?  Couldn't you use two motors and then some type of center caster wheel or something and then do tank controls?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colecago
    colecago over 12 years ago

    Putting motors in parallel off a single drive doesn't work well.  Motors are pretty dynamic devices and if one stalls it will take all the current from the other one in parallel causing weird behavior.  Why are you using 4 motors instead of 2 anyways?  Couldn't you use two motors and then some type of center caster wheel or something and then do tank controls?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to colecago

    the reason i'm using 4 wheels is because in the competition, the robot has to climb a 15 degree incline to pick up a box. My current robot is 2 wheels and I tried to climb it on the incline, but it couldn't climb it. Does that mean, I have to use two motor drives, to operate the 4 motors??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colecago
    colecago over 12 years ago in reply to e14 Contributor

    Well you probably won't hurt the driver chip, but it might not work properly, so I'd say try it.  If they aren't loaded too heavily it might work okay, but in general you don't want to put two brushed motors in parallel when each experiences differing loads.