element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum RPI monitor
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 31 subscribers
  • Views 707 views
  • Users 0 members are here
Related

RPI monitor

royston02
royston02 over 12 years ago

I want to use a monitor with a VGA input. I found this one-

Zebronics 15 6” LED Monitor 3 YRS Warranty Sealed Pack VAT Bill | eBay

I don't know 2 things,

-if it will interface with the pi

-what is the input voltage

  • Sign in to reply
  • Cancel
  • johnbeetem
    johnbeetem over 12 years ago

    RasPi can talk to a VGA monitor through an HDMI->VGA converter box.  There are some issues with this, which are described in the RasPi Hardware Wiki:

     

    http://elinux.org/RPi_Screens#RGB_analog.2FVGA

    http://elinux.org/RPi_VerifiedPeripherals#HDMI-.3EVGA_converter_boxes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • royston02
    royston02 over 12 years ago in reply to johnbeetem

    On the monitor its given dc so I don't know how much Vs to supply it because I want to plan everything in advance

    secondly, I found this one-

    http://www.ebay.in/itm/HDMI-to-VGA-Converter-With-3-5MM-Audio-for-HDTV-Monitor-Projector-A002-/380803161245?pt=LH_DefaultDomain_203&hash=item58a9a31c9d&_uhb=1#shpCntId

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • royston02
    royston02 over 12 years ago in reply to johnbeetem

    I also found this

    -http://www.ebay.in/itm/1080P-Mini-HDMI-Male-to-VGA-Female-Adapter-Video-Converter-3-5mm-Audio-Output-/161202113378?pt=LH_DefaultDomain_203&hash=item2588650b62&_uhb=1#shpCntId

    -http://www.flipkart.com/jinali-hdmi-male-vga-female-sound-data-cable/p/itmdsa2fgafrh7gb?pid=ACCDSAFAFZ33SWZS&otracker=from-search&srno=t_4&query=hdmi+to+vga+&ref=530e8917-b0de-4e9f-a246-cf7ee0428660

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to royston02

    royston dsouza wrote:

     

    On the monitor its given dc so I don't know how much Vs to supply it because I want to plan everything in advance

    secondly, I found this one-

    http://www.ebay.in/itm/HDMI-to-VGA-Converter-With-3-5MM-Audio-for-HDTV-Monitor-Projector-A002-/380803161245?pt=LH_DefaultDomain_203&hash=item58a9a31c9d&_uhb=1#shpCntId

    The eBay page shows a picture of a power supply and VGA cable, so I would hope that the vendor includes a compatible power supply so you don't really need to know what the DC voltage/current is.  However, it would be worth checking that they do include the power supply.

     

    Regarding HDMI-to-VGA converters in general: if you read the RasPi Hardware Wiki pages that I linked to, you'll find that getting a compatible converter can be problematic.  For best results, get one for which someone has already reported RasPi success.  Otherwise, you may need to play hardware and configuration games to get it to work.  I'd be very careful with a self-powered converter like the one shown above.  RasPi provides 5V to on its HDMI connector through a BAT54 diode D1 which has a 200 mA max rating.  If the adapter needs more than that, D1 may burn out.  There's a good discussion of this at the RasPi Forum: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=9819

     

    So, if you need to get a converter that doesn't have a track record with RasPi, it's probably best to get something with an external power input.  But do expect to have to play with config.txt to get it working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    The monitor will just connect to about any  power outet, between 110 and 220v, the power conversion is made inside of the device. The only problem you might have is the rasPi video output that is either composite or hdmi; buy a dongle to covert hdmi to vga and use a 3.5mm jack to output the sound.  image