element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Need Advice - DIY Sea Turtle Nest Temperature Logger
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 33 subscribers
  • Views 2025 views
  • Users 0 members are here
Related

Need Advice - DIY Sea Turtle Nest Temperature Logger

e14 Contributor
e14 Contributor over 12 years ago

Hey y'all,

 

I'm hoping the title caught your attention. I'm a graduate student looking to assemble temperature data loggers, which will be buried in the sand for approximately 2 months. They run about $40 from established companies, but I would not have the funding to buy enough. I figured the DIY approach could produce the same results.

 

Standalone Temperature/Voltage Logger « insideGadgets

This is essentially what I'm looking to produce. Although with this kit I would need to improve the thermistor to one that has an error of 0.5 degrees Celsius.

 

The data logger would need to be weather-proofed, as it's going to be coated in sand, with the possibility of water. However, I do need to access the data later.

 

Any and all advice would be greatly appreciated.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thanks for all the support guys. I really appreciate the contribution y'all are making by at least with regards to brainstorming.

     

    Great concept Tim, but it might be a little bit more advance to what I would like to accomplish.

     

    With direct response to Michael, I do have some experience with breadboarding and soldering. So that in itself wouldn't be an issue. I've never really had a hand in coding, but I do have some potential resources around me that might be willing to help out.

     

    I'm still working out the kinks to the whole project design, but my projected budget that the university is willing to provide is US$500. That severely limits my options, but I am willing to personally contribute to this research to ensure it gets completed. If I could get 50 data loggers at US$10 a pop, I would be ecstatic. Realistically, I'm thinking that 20-25 data loggers will suffice, and I will have to utilise each data logger twice to get a decent enough sample size.

     

    The film canisters are a great idea, as I don't want to disrupt the sea turtle nest in itself while collecting these measurements.

     

    vsluiter:

     

    From what I understand, most of these devices use a coin cell battery, which should be able to power the device at least 6 months, using 1 minute intervals. I would be collecting these measurements at 1-4 hour intervals; it hasn't been decided yet. This is in turn would increase the length of the battery life.

     

    The temperature collected would be around 28-30 degrees C, which is 82-86 degrees F.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thanks for all the support guys. I really appreciate the contribution y'all are making by at least with regards to brainstorming.

     

    Great concept Tim, but it might be a little bit more advance to what I would like to accomplish.

     

    With direct response to Michael, I do have some experience with breadboarding and soldering. So that in itself wouldn't be an issue. I've never really had a hand in coding, but I do have some potential resources around me that might be willing to help out.

     

    I'm still working out the kinks to the whole project design, but my projected budget that the university is willing to provide is US$500. That severely limits my options, but I am willing to personally contribute to this research to ensure it gets completed. If I could get 50 data loggers at US$10 a pop, I would be ecstatic. Realistically, I'm thinking that 20-25 data loggers will suffice, and I will have to utilise each data logger twice to get a decent enough sample size.

     

    The film canisters are a great idea, as I don't want to disrupt the sea turtle nest in itself while collecting these measurements.

     

    vsluiter:

     

    From what I understand, most of these devices use a coin cell battery, which should be able to power the device at least 6 months, using 1 minute intervals. I would be collecting these measurements at 1-4 hour intervals; it hasn't been decided yet. This is in turn would increase the length of the battery life.

     

    The temperature collected would be around 28-30 degrees C, which is 82-86 degrees F.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • vsluiter
    vsluiter over 12 years ago in reply to e14 Contributor

    Hi Diverdan,

    Nice project... If you want it to succeed, think about what you need first (sample rate, needed accuracy, how to get data off the device), and then start developing. Changing specs along the way is a surefire way to go outside space / time / money budget.

    By the looks of your numbers you want to have useful data between 28 and 30 degrees; with 0.5° resolution, that would only give 5 values. Do you need a larger range, or a more precise sensor? I've once made a circuit that was measuring within 0.1° Celsius over a range of -5 to 40°C, and in hindsight I think I could better have bought one of these sensors: http://www.ist-usadivision.com/sensors/temperature/tsic-sensors.php

    The reason I warn about battery usage is that it's very hard to get to low power usage if you don't take it into consideration from the start of your product design. You can easily get this started while not paying attention to it, but it'll be much harder to get to a lower consumption from that point, than it is to first start at very low power consumption, and gradually add features. Then you'll also be able to see what feature is affecting the current consumption.

    Read this: Making the Arduino sleep the long sleep and this: https://www.sparkfun.com/tutorials/309 for more info on making Atmels sleep.

     

    Good luck with your design, it would be nice if you kept us posted!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to e14 Contributor

    Here are some component ideas:

    Temperature sensor: TI TMP112AIDRLT (Farnell 1735574 @ £1.41) - 10uA active, 1uA shutdown, 0.0525C resolution, typical accuracy 0.1C worst case 0.5C.

    Micro: LPC811M001 (Farnell 2320693 @ £0.56), ARM M0, 16 pin, low power modes, cheap

    Real time clock: Microchip MCP7940N (Farnell 2361116 @ £0.49)

    EEPROM: Microchip 24AA128 (Farnell 1331285 @ £0.43)

    Battery: CR2450, about £1.50 (don't buy junk)

    Battery holder, about £0.25.

    Each time the recorder wakes up to measure it must be on for about 100mS to measure temperature and will use max 2mA, then write to EEPROM for 5mS using 5mA = 0.225mAS.

    If it does once per minute the average current drain is 3.75uA.

    Allow the RTC to use 2uA (way more than spec) gives an average current drain of 5.75uA

    The battery is good for about 500mAH (depends on which you get) so the battery will do 86,000 hours.

    You might be tempted to use a smaller battery but aim for 10x the calculated capacity - you really don't want to run flat for the sake of 25p.

    You can get the data out of the uP by a uart interface using one of those FTDI logic level uart to USB cable thingies which work with almost any Windows PC.

     

    By the time you get the pcb, crystal etc I reckon the total materials cost will be about £9, about $15.

     

    Sounds such fun I quite fancy making one myself but I'd better get on with some real work image

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to michaelkellett

    Nice breakdown!

    Since they've got such good documentation I'm advocating the use of the Zero Gecko with internal RTC (EFM32ZG108F160.9 μA @ 3 V Deep Sleep Mode, including RTC with 32.768 kHz) and replacing EEPROM by FRAM. But of course that's personal favourism and some overoptimization, Michaels setup seems very good too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to vsluiter

    The Gecko has the RTC on chip so would save the external RTC and so the BOM would reduce a bit - which is good. I picked the NXP LPC800 part because it's in an easy to solder package (and I didn't know about the Geckos - never used them).

    I think the Gecko is a better choice than the NXP part if the package is OK - I don't mind QFNs but I know that some hand solderers can't manage them.

    I chose the EEPROM because I wanted everything to work down to 2V (you can't trust coin cells to give you any more over their life and a reasonable temperature range) - have you a part number for a FRAM ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to michaelkellett

    Yes, you can look at this Ramtron part http://nl.farnell.com/ramtron/fm25640b-g/fram-64k-spi-8soic/dp/2077754 or at Cypress's parts : http://www.cypress.com/?mpn=FM25V01-G . I see now that they are waaay more expensive though , and thus mot particularly suited to your project.

    There's some background info here too: http://www.ti.com/lsds/ti/microcontroller/16-bit_msp430/fram/overview.page?DCMP=FRAM&HQS=FRAM. The low power properties are especially useful if (re-)writing large chunks of data, which you are not going to do. TI makes the MSP430 (low power micro) also with internal FRAM, but I don't know if it would suffice for your purpose. This one has 16kByte storage (used for both data and program): http://nl.farnell.com/texas-instruments/msp430fr5728irget/ic-mcu-16bit-msp430-24vqfn/dp/2072183 . The interesting thing is that you have a low power microocontroller with nonvolatile storage and an RTC in one package. Still more expensive than Michaels options, but you'll have to place only one part....