element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum My arduino car project.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 29 subscribers
  • Views 595 views
  • Users 0 members are here
Related

My arduino car project.

yawgyakobo
yawgyakobo over 12 years ago

HELLO.

I am making an arduino car project and I am using an arduino Mega ,a motor shield  , two solar panels and two 9 volt batteries. I am planning to attach solar panels and the two 9 volt batteries straight to the arduino motor shield. I think I should use a type of resister to minimise the flow of electricity , but what kind of resister should I use or should I add an automatic rechargeable device.  

  • Sign in to reply
  • Cancel

Top Replies

  • jadew
    jadew over 12 years ago +1
    Hey, usually motors take just what they need, if you supply them with the right voltage, so you probably need a voltage regulator and a brown out detector so you cut the current when the voltage is below…
Parents
  • jadew
    jadew over 12 years ago

    Hey, usually motors take just what they need, if you supply them with the right voltage, so you probably need a voltage regulator and a brown out detector so you cut the current when the voltage is below the minimum threshold.

     

    You should worry about what happens when they get stuck, in which case they'll start drawing as much current as the wire resistance allows it. You don't want to limit the current flow, but actually completely cut it, or cut it for a while and then reverse it (in an attempt to get unstuck). Since lower current won't get it unstuck and maintaining power while stuck, can fry it, you need a way to detect over current and act on it fast.

     

    To detect over current you can use a comparator (some AVRs have one or two on board) and feed the output to the MCU, it should be able to handle it fast enough before any damage is done to the motor, but extra care must be taken so you make sure the code doesn't get interrupted for too long or that it gets run with too much of a delay. Once the AVR is notified, it can either cut current to the motor or it can go trough some movement pattern to unstuck it and if that fails it eventually gives up and cuts the current.

     

    As an extra precaution, you can use the humble fuse, a slow blow fuse with the appropriate current rating should do the job and protect at least the motor and the batteries from getting fried.

     

    I hope this answered your question.

     

    Edit: I don't know what kind of motors and solar panels you have, but generally speaking you need a fairly big panel to drive even a low power motor. Solar panels are normally used to recharge a rechargeable battery, rather than to drive a heavy load directly.

     

    Razvan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jadew
    jadew over 12 years ago

    Hey, usually motors take just what they need, if you supply them with the right voltage, so you probably need a voltage regulator and a brown out detector so you cut the current when the voltage is below the minimum threshold.

     

    You should worry about what happens when they get stuck, in which case they'll start drawing as much current as the wire resistance allows it. You don't want to limit the current flow, but actually completely cut it, or cut it for a while and then reverse it (in an attempt to get unstuck). Since lower current won't get it unstuck and maintaining power while stuck, can fry it, you need a way to detect over current and act on it fast.

     

    To detect over current you can use a comparator (some AVRs have one or two on board) and feed the output to the MCU, it should be able to handle it fast enough before any damage is done to the motor, but extra care must be taken so you make sure the code doesn't get interrupted for too long or that it gets run with too much of a delay. Once the AVR is notified, it can either cut current to the motor or it can go trough some movement pattern to unstuck it and if that fails it eventually gives up and cuts the current.

     

    As an extra precaution, you can use the humble fuse, a slow blow fuse with the appropriate current rating should do the job and protect at least the motor and the batteries from getting fried.

     

    I hope this answered your question.

     

    Edit: I don't know what kind of motors and solar panels you have, but generally speaking you need a fairly big panel to drive even a low power motor. Solar panels are normally used to recharge a rechargeable battery, rather than to drive a heavy load directly.

     

    Razvan