element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Like-a-pro soccer display?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 33 subscribers
  • Views 2648 views
  • Users 0 members are here
Related

Like-a-pro soccer display?

e14 Contributor
e14 Contributor over 12 years ago

Dear Ben,

I would love to make something special for the non professional soccer team my son plays for.

How difficult would it be to create a large (7-segment led ?) display the coach could use to call for players' substitutions during a match?


Design requirements:

-to have two pair of 2 digits separated by ":" (first pair red, second green)

-to be big/bright enough to be readable from 30 yards/meters in sun light

-to use self contained energy (a battery I suppose)

-to be portable, light and sturdy in the same time

-to be low cost

-to be easy to operate

 

Thank you in advance,

Carlo

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    You could make your own 7-segment with discrete LEDs on PCB or stripboard. Use a transistor per segment and drive it from any small micro-controller board. You can buy large 7-segment displays. Here's…
Parents
  • shabaz
    shabaz over 12 years ago

    Hi Carlo,

     

    It may be worth purchasing a single LED digit, and testing it out. I did a similar thing, but for indoor game use in a bright environment. I used Avago HDSP-N150 which are 0.8 inch high digits, and were very bright and readable from 10 meters away. I think you will need larger digits. There are quite a few larger displays such as this one, but it's not mentioned in the datasheet how far away it is readable.

    Also, you'll need some sort of filter. I used this filter sheet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    thank you but I think I need a much larger display. the professional ones are 10+ inch high

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    You could make your own 7-segment with discrete LEDs on PCB or stripboard. Use a transistor per segment and drive it from any small micro-controller board.

     

    You can buy large 7-segment displays. Here's an 8" model from Seed studio, although it doesn't seem to be available to order:

    http://www.seeedstudio.com/depot/7-Segment-Display-8-Inches-Red-p-1194.html

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    ciao pigraham, do you think possible to control 4 of those displays using an Arduino Uno? Please forgive me but I'm not an expert.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colecago
    colecago over 12 years ago in reply to e14 Contributor

    They do make them, I've seen them at my local hackerspace, you'd have to contact them.  I'm sure they are out of your price range though, one of their failings was price because recreational sports teams don't want to spend a lot of money on such a thing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • benheck
    benheck over 12 years ago in reply to colecago

    It's kind of hard to make a large display affordable / automatic.

     

    A mechanical display with electromagnetic flaps to create letters is best for readability, but even more expensive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Yes, I'm sure an Arduino Uno could control 4 seven segment displays.

    All you have to do is use MOSFETs to handle the current (too much for a logic GPIO pin).

    The UNO has 14 I/O and there are 28 segments to control (4x7), but you can multiplex.

    Use 4 lines to drive high-side switches on each of the 4 displays.

    Use 7 lines to drive N-channel MOSTFETs  to pull  the cathode of a segment on each display to GND.

    Write code do do this:

    turn on display 1 and set the segment controls for the first digit .

    Turn off display1

    turn on display 2 and set the segment controls for the second digit .

    Repeat for all 4 digits.

     

    You could build segments on strip board and attach those to a backboard.

    Alternatively you could drill holes in a board in 7-segment pattern and glue lots of LEDs in the holes. Wire up the LEDs pin to pin and connect to the switching circuit on a Proto Shield.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Here's an LED board

    FAVERO: Football/Soccer Substitution Boards, Substitute Boards, Player Substitution, Extra Time Board, Player Substitute

     

    €300

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I think I need a stroke of our Ben-genius!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I think I need a stroke of our Ben-genius!