element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum idea for a build
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 30 subscribers
  • Views 857 views
  • Users 0 members are here
Related

idea for a build

vinceverc
vinceverc over 12 years ago

hello ben is it possible to build something that gives your plants water when you are not a home?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    It would be very possible to build an automatic plant watering machine.

     

    You would need to have a tank to store the water, and some method of letting it out, possibly a solenoid valve. Maybe one of these valves would work for you. SY114-VLOZ-Q - SMC SY114-VLOZ-Q - VALVE, 3 PORT, CLOSED, 6DC | Newark element14 Canada.

     

    You would also need some method of sensing the level of the water, possibly, if you were to use a water level float sensor in a pipe that is inserted in the dirt, this may work. Liquid Level Sensors - Float | Newark element14 Canada

     

    Lastly, you will need the some sort of micro-controller that can communicate with the sensor and valve.

     

    If you wanted to do this for many plants, then you would probably want to have individual valves and sensors.

     

     

     

    This might not be the best way to do it, but it might work.

     

     

     

     

    ~Sehr Ludwig

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • royston02
    royston02 over 12 years ago in reply to e14 Contributor

    The best thing to do is to use drip system which will help you water the plants whether you're or aren't at home. way better then watering plants manually. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to royston02

    That is true too, there are always those glass balls with a spout that you stick in the dirt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    It should be pretty easy to use a micro controller with a electronically controlled valve and some type of moisture sensor. The micro controller can measure the moisture levels in the soil ever x-time interval and if the levels are below a certain amount the controller can turn on the water valve for an interval of time before turning itself back off. How the watering system would work could be up to you, but its possible to pipe it right into the houses water supply so you wouldn't need to ever refill the system and you would just have to check up on it to make sure nothing broke and your plants are healthy. I've seen some projects that use the arduino uno and an orbit 62035 hose water valve or adafruit sells a Plastic Water Solenoid Valve, which may be a better choice for an easier electronics setup but slightly more work in the piping works. This combined with something like the adafruit Soil Temperature/Moisture Sensor could be just what you are looking for. Although it take a decent amount of coding, and I am not positive if the orbit62035 can be ran straight from the arduino pin outs. Hope this helped!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Ben when you are building the plant waterer system, can you use a 555 timer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    It is a great idea to have it piped from the house, the only problem that would have to be watched out for is that if you have the pipe into the water, if the water pressure drops somehow (especially if you are on a well system), then you couls suck the water from the plant back into the system.

     

    I would suggest that it drips onto the plant to prevent this; clean drinking water is always a good thing to have.

     

     

     

    ~Sehr Ludwig

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I agree, in my mind I was designing it as if it were a shower head... probably should have mentioned that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    That is a great idea! I don't know what having a shower head would look like though, maybe if you have it poor into a funnel, then have the funnel piped into the plant, that way you can hide the funnel, and not have as bad of a risk for back washing.