element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum LEDs-based desk lamp
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 29 subscribers
  • Views 1015 views
  • Users 0 members are here
  • desk
  • led's
  • lamp
Related

LEDs-based desk lamp

rabr2ro
rabr2ro over 12 years ago

Hello Ben,

 

I think for a while, if I should bother you with my proposal and finally I did it. Currently, I'm working on a similar project (I'm in design phase), but I found on the internet only pieces of information that I had to put them together, so I would like to see how this can be done. Plus, it might be useful and fun for a lot of peoples, especially if they design it as they like. So this is my project proposal:

- to make a desk lamp (from scratch or using scrapped parts) that uses bright (power) LED's; in my project I use 27 while LED's (OVA-1081) bought from element14; LED's can be arranged on a disk, but any shape will do.

- initially I intended to make a capacitor-based power supply (aka “transformer-less” power supply) to provide power to the LED's from house outlet (230V, 50Hz), but the information that I could found to build such a power source were very thin, the risk to electrocute myself very high (or even worse, to fry the electric network of the entire block), so I decided to use a laptop power supply (output 12V, 2A). You can build it as you see fit, I'm hopping for a third idea.

 

Optionally, additional functionality can be added:

- a potentiometer can be installed to adjust the light intensity, if is desired

- add some intelligence with an Arduino and some sensors, like: turn on/off swiping over a specific area, or automatically turns on when you set at the desk and turns off when you leave the desk and light in the room in under a specific level, etc. For a first version, I can leave without optional points, but it's up to you if you want to add some "personality" to your build image


Thank you for reading my proposal and I hope to see the video soon image

Radu

  • Sign in to reply
  • Cancel
  • colecago
    colecago over 12 years ago

    I built this rudimentary light using a teensy and one of those promotional highlighters that was going to waste.  I ended adding 4 potentiometers, one controlled the max brightness, one controlled the fade timing, one controlled the overlap of the fade in/fade out, and one controlled another timing aspect that I don't recall.  I should really do a write up on it.

     

    https://www.youtube.com/watch?v=MkbV-fM24co

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sophiaedward64
    sophiaedward64 over 7 years ago

    I hope you have bought.