element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 3d Printing a circuit board
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 30 subscribers
  • Views 418 views
  • Users 0 members are here
  • 3d-printing
Related

3d Printing a circuit board

e14 Contributor
e14 Contributor over 12 years ago

Hi

This idea came up to me, when I saw your two headed 3d printer. The basic idea is to use one of the head to print the plastic board and the other head to print a thin layer of solder .

Both surface mount and through hole devices can be used on such a board.

image

 

WORKING (AS I IMAGINED image)

First the Head 1 prints the plastic part of the PCB, leaving small thin dents on the surface where the copper should go.

Second Head 2 with solder as its input , melts and puts a thin layer of solder where the copper should be.

So now we have a base with a conducting path. This should work as a simple PCB.

This is just my idea, more inputs are welcome, to better it, one day we could be able to print arduino(s) out a 3d printer. image


regards


  • Sign in to reply
  • Cancel
  • antoinec
    antoinec over 12 years ago

    Seems like a great concept to me. But then you shouldn't use regular PLA or ABS because I reckon the plastic would melt when the hot solder is put on top of the plastic.

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colecago
    colecago over 12 years ago

    Solder has like no strength and won't stick to the plastic.  The first component you try and solder on would ball up and destroy the solder trace.  You are probably better off printing some type of conductive epoxy and then use the same type of stuff to glue the leads to the traces.