element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Unlimited free electrictiy!!!!!!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 32 subscribers
  • Views 883 views
  • Users 0 members are here
Related

Unlimited free electrictiy!!!!!!

david98xp
david98xp over 11 years ago

This video is amazing breaking the laws of physics. Simply use magnetics to keep a motor spinning. Why don't we use this? Are the power companies hiding something?

 

 

Free Energy Magnet Motor fan used as Free Energy Generator "Free Energy" light bulb - YouTubehttp://www.youtube.com/watch?v=jiAhiu6UqXQ

  • Sign in to reply
  • Cancel
Parents
  • supper_slash
    supper_slash over 11 years ago

    I think this video enplanes the problem with this theory best.

    Just for the record, i do not have neo, mags, but, i did hot glue some mags to an old fan to see if i could get it to spin freely, and i ran in to the same problem noted into this video, i could not get the fan to spin freely at all, like in the original posted video.

    I think there is something fishy going on with the video, the mags, seam to react to the fan out of ordinarily.

    Also, just for kicks, i used compressed air to spin the fan up to 3000 rpm (way faster than in the first video) and i was getting an ac 2.3461 V @ .0432A

    So, it don't seam to be a viable power source for a light bulb, that was powered off of a dc battery.

    Although, i suppose, an led, would rectify the power and give off light.image

    Hum.....??

    Would it?

    Anyone  care to comment on that? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to supper_slash

    This is just another twist on a perpetual motion machine scam. One thing I noticed was that the speed of the spinning fan did not slow when the bulb was attached. If the fan was producing the power it would have loaded down when the bulb was attached just like I slow down on my bicycle when I come to a hill. We have to always ask ourselves where is the energy coming from. In this case we have a fan spinning and a light giving off photons. The problem with the magnet idea is that the hand magnet is pushing the next magnet in line away with the same force it is pushing the first magnet away and this produces an equilibrium of forces and no net rotation. I would go looking for batteries and a switch. It is doubtful that the disks on the fan blades are even magnets. DAB had it right on the money, nothing free.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 11 years ago in reply to jw0752

    Hi John,

     

    On a side note, I show how you can get perpetual motion in a photon in my book.

    It really can be done, it just has no practical value to generate any useful energy.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to DAB

    HI DAB - Yes when we get to the quantum level somethings seem to be in perpetual states. A super conductor will maintain a current and a magnet field indefinitely as long as we can keep the environment from destroying the state of super conductivity. The dificulty is always how to get usable energy out of a system. Useful energy always has to come from somewhere, either from the conversion of another state of dynamic energy or from the conversion of what is refered to as potential energy. The free energy people always want it to come magically from magnetism or gravity and while potential energy can be stored in magnetic fields and gravitaional fields it has a book keeping system that always costs something from the entire system.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 11 years ago in reply to jw0752

    Yes, mass and energy are 100% conserved.

    The cool thing was that I was able to resolve entropy in Thermodynamics.

    The early experiments only looked for thermal energy and mass.  When you realize that thermal flow like electric charge flow are the same, so you get more than just thermal photons.

    The movement of mass/energy between atoms is really amazing when you look at it from the subatomic level.  It all makes sense.  You are just dealing with mass/energy differences between the electron clouds.  The photons move back and forth until the adjacent atoms are all at the same state.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 11 years ago in reply to jw0752

    Yes, mass and energy are 100% conserved.

    The cool thing was that I was able to resolve entropy in Thermodynamics.

    The early experiments only looked for thermal energy and mass.  When you realize that thermal flow like electric charge flow are the same, so you get more than just thermal photons.

    The movement of mass/energy between atoms is really amazing when you look at it from the subatomic level.  It all makes sense.  You are just dealing with mass/energy differences between the electron clouds.  The photons move back and forth until the adjacent atoms are all at the same state.

     

    DAB