element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum its possible to interface bluetooth mtb-503-03 device with arduino
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 29 subscribers
  • Views 987 views
  • Users 0 members are here
Related

its possible to interface bluetooth mtb-503-03 device with arduino

e14 Contributor
e14 Contributor over 11 years ago

help me to find it

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 11 years ago +1
    Should the part number be MBT-503-03 ? This seems to be a USB bluetooth dongle - if you want to plug it into an Arduino, you would need a USB OTG module for your arduino. I can't tell if it is really a…
Parents
  • gihu
    gihu over 11 years ago

    Hi,

     

    There are USB Host Shields, I do not know if USB dongles are supported, but probably much software will be required.

    Although it seems someone get it:

    Using USB Bluetooth dongle on Arduino to connect to Android phone « Circuits@Home

    Therefore, It would be much easier using UART to Bluetooth modules like HC-05, or RN42 from microchip.

    The shields have a dedicated chip for the usb host, and it is connected to the arduino over SPI, so probably much software is required.

    Using HC-05 or RN42 simple use of UART of the arduino is needed.

     

    Hope that helps,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gihu
    gihu over 11 years ago

    Hi,

     

    There are USB Host Shields, I do not know if USB dongles are supported, but probably much software will be required.

    Although it seems someone get it:

    Using USB Bluetooth dongle on Arduino to connect to Android phone « Circuits@Home

    Therefore, It would be much easier using UART to Bluetooth modules like HC-05, or RN42 from microchip.

    The shields have a dedicated chip for the usb host, and it is connected to the arduino over SPI, so probably much software is required.

    Using HC-05 or RN42 simple use of UART of the arduino is needed.

     

    Hope that helps,

    Miguel