element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Battery charging circuit for more than one cell?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 31 subscribers
  • Views 1176 views
  • Users 0 members are here
  • lipo
  • charger
Related

Battery charging circuit for more than one cell?

e14 Contributor
e14 Contributor over 11 years ago

I was very excited when I heard that Ben Heck was about to make a Video about Battery Charging Circuits, but my hope that he would show us a circuit to charge multiple cells wasn't fulfilled. So, I'm working on a Project that requires a 4s to 5s Lipo Battery and I have no idea how I should work this out. Could anybody help me out on this one? Most confusing for me is that I need an Output Voltage of 18.5V (5s) but to charge I need 4.2V on every Cell. How can this be done?

 

Thanks in Advance for any Help!!

  • Sign in to reply
  • Cancel
Parents
  • vsluiter
    vsluiter over 11 years ago

    Florian,

     

    Please be very careful when charging LiPo's!! Back in the day that NiMH was the 'leading' chemistry, you could easily make charger by making a constant current source. If you had a string of batteries, and one of them would get a lower capacity during use you could 'balance' your pack again by overcharging the pack; the pack would get hot, but no bad things would happen. Please read this on balancing: Balancing Li-Po Battery Packs - How and Why

    Everything Lithium-rechargeable should be handled with care!! Overcharging is not an option as your pack might explode. Cell voltages need to be carefully checked during charging, and the charging algorithm is a bit more complex than NiMH (first constant current, than constant voltage charging).

     

    Now for your solution: you could either try the approaches in this document by Adafruit (PDF): https://learn.adafruit.com/downloads/pdf/multi-cell-lipo-charging.pdf , where each battery gets charged by its own charging circuit, or build your own system (which I advice against if you're not experienced in electronics).

     

    Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • vsluiter
    vsluiter over 11 years ago

    Florian,

     

    Please be very careful when charging LiPo's!! Back in the day that NiMH was the 'leading' chemistry, you could easily make charger by making a constant current source. If you had a string of batteries, and one of them would get a lower capacity during use you could 'balance' your pack again by overcharging the pack; the pack would get hot, but no bad things would happen. Please read this on balancing: Balancing Li-Po Battery Packs - How and Why

    Everything Lithium-rechargeable should be handled with care!! Overcharging is not an option as your pack might explode. Cell voltages need to be carefully checked during charging, and the charging algorithm is a bit more complex than NiMH (first constant current, than constant voltage charging).

     

    Now for your solution: you could either try the approaches in this document by Adafruit (PDF): https://learn.adafruit.com/downloads/pdf/multi-cell-lipo-charging.pdf , where each battery gets charged by its own charging circuit, or build your own system (which I advice against if you're not experienced in electronics).

     

    Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • royston02
    royston02 over 11 years ago in reply to vsluiter

    No offenseto element 14. On adafruit, you get Lipo cells of 2500mah. There are also these chrgers-micro coonneter Lipo chargers. You could make a toogle switch and choose when to give output. connect in series and it will give required voltage. When you input the chrging point, rather than using 4 micro usb cables, use one which can provide 2-2.5 amps and connect it to all of them. The charger let's you choose when to give output via a pin as well as tells you when a cell is low. I'm going to use it my self in a future project andconnect in parellel rather than series.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to vsluiter

    vsluiter: I know of the dangers of the LiPo-Cells,thats why I am asking you for help here. I use them a lot on other projects, but always that way that I was unplugging them and put them on a dedicated LiPo-charger.

    Now I'm planning something like Ben's mobile gamingstations, but it should be battery powered too.

     

    @royston dsouza: I know of the guide from Adafruit and already read them, but my problem with this setup is, that I can't use the system while charging it. Other than that, it would work for me.

     

    Does anybody have a solution to this problem?

    Isn't there a charger IC available for, lets say 6 Cells wich will balance charge? Like the one Ben used in his charger circuit?

     

    Thank You!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 11 years ago in reply to e14 Contributor

    Hi Florian.

     

    I quickly looked at Linear and TI's  website. As far as I can see it will be a two-fold design approach; you'll need a charger that provides enough voltage / current, and you'll need a solution to monitor  each cell's voltage. I think most 'straightforward' designs are built up this way. If you want to go fancy (and / or care about battery life) you could also add cell balancing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • royston02
    royston02 over 11 years ago in reply to vsluiter

    On adafruit, there are special charger boards that allow you to charge and run at the same time.