element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Burglar Alarm to Door Buzzer Using a Monostable Circuit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 31 subscribers
  • Views 4399 views
  • Users 0 members are here
  • monostable
Related

Burglar Alarm to Door Buzzer Using a Monostable Circuit

e14 Contributor
e14 Contributor over 11 years ago

At work we are currently using what I suspect is a burglar alarm as a door buzzer. It's inappropriately loud to have buzzing the entire time the door is ajar (from barely open onward), as we're a motel and it's frankly obnoxious. However in order to hear people come in from the basement, it's what the folks in charge decided to use. I would very much like to create a monostable circuit so it buzzes for a small amount of time then turns off until the door is shut again, re-arming the buzzer. The buzzer works using a momentary switch that is pressed when the door is shut and released when the door is open. This switch is connected to what looks like a transformer core, and the device also plugs into our AC outlet.

 

I have looked at circuits online, but even using a few simulators I was unable to produce results like I wanted. Can I have some advice? I'm new to electrical engineering.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1
    Hi Simon, I have set up a mock up of an improved circuit which allows the door switch to close and remain closed. The components that I have selected for C1 and R1 give a time of approximately 5 seconds…
Parents
  • D_Hersey
    D_Hersey over 11 years ago

    Another way to go would be to detect the sounding of the buzzer would be to attach the series combination of a resistor, a half-wave bridge rectifier and the B-E junction of an NPN (E attaches to BOS) transistor.  The collector is connected to TOS through a resistor.  This node goes low when the buzzer sounds, except during the zero-crossings.  An opto-isolator could be used instead here, BTW, shunt the input LED with a reversed signal diode.  So, these zero crossings occur at a rate 2x the line fq.  We can count-and-compare for our duty pulse, ultimately connecting to a relay as John describes.

     

    John's way works:  Using the 555 in the datasheet way is considered unstylish in some design circles, but that's no nevermind.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 11 years ago

    Another way to go would be to detect the sounding of the buzzer would be to attach the series combination of a resistor, a half-wave bridge rectifier and the B-E junction of an NPN (E attaches to BOS) transistor.  The collector is connected to TOS through a resistor.  This node goes low when the buzzer sounds, except during the zero-crossings.  An opto-isolator could be used instead here, BTW, shunt the input LED with a reversed signal diode.  So, these zero crossings occur at a rate 2x the line fq.  We can count-and-compare for our duty pulse, ultimately connecting to a relay as John describes.

     

    John's way works:  Using the 555 in the datasheet way is considered unstylish in some design circles, but that's no nevermind.