element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Burglar Alarm to Door Buzzer Using a Monostable Circuit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 31 subscribers
  • Views 4414 views
  • Users 0 members are here
  • monostable
Related

Burglar Alarm to Door Buzzer Using a Monostable Circuit

e14 Contributor
e14 Contributor over 11 years ago

At work we are currently using what I suspect is a burglar alarm as a door buzzer. It's inappropriately loud to have buzzing the entire time the door is ajar (from barely open onward), as we're a motel and it's frankly obnoxious. However in order to hear people come in from the basement, it's what the folks in charge decided to use. I would very much like to create a monostable circuit so it buzzes for a small amount of time then turns off until the door is shut again, re-arming the buzzer. The buzzer works using a momentary switch that is pressed when the door is shut and released when the door is open. This switch is connected to what looks like a transformer core, and the device also plugs into our AC outlet.

 

I have looked at circuits online, but even using a few simulators I was unable to produce results like I wanted. Can I have some advice? I'm new to electrical engineering.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1
    Hi Simon, I have set up a mock up of an improved circuit which allows the door switch to close and remain closed. The components that I have selected for C1 and R1 give a time of approximately 5 seconds…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Relay it is. I keep putting more than 1W through the simulated buzzer and destroying it (no idea what the real one can handle). The transformer seemed to be building up voltage, but with this configuration it does not. Am I the only one who thinks the transformer reverse connections are odd? Maybe it's a common thing to do.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    Hi Simon, Your present real life transformer buzzer arrangement has proven functionality. I would not change anything there except to use the relay for the switch in place of the door switch which will go to triggering the 555 circuit. The D-2 in your latest schematic is a mistake and should not be used as it will tie your low voltage to your mains. I would put the relay switch into the circuit on the same side of the transformer as the buzzer and leave the transformer hooked directly to the mains. I am not sure but this is probably the way it is hooked up in your present real life application as it is the safest and most professional way to hook it up. The transformer relay part of the circuit does not have polarity ( + signs ) as it is AC.  At this point don't worry about the power handling ability of the buzzer as your simulation buzzer may not accurately emulate the real one. I also see that you have upped the R-1 to give yourself about 1 second of buzzer when the door is open. This is probably a good idea. Now it is time to get your schematic approved and build it. I am looking forward to good results.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to jw0752

    What do you mean by "use the relay for the switch in place of the door switch"? I'm hesitant to mess with the door switch, as it took three iterations for the electrician to get one that was reliable installed. They would work for a few times then stop working, and the current one has remained working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    Sorry if I confused the issue. Leave the door switch as it is in the door but run the wires from it to the switch position in our schematic. Run the wires from the relay contacts to the position in the old door bell circuit where the door switch was originally. Here is a revised and completed schematic of how your system should look.

    John

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    Hi Simon, The relay should be rated at about 9 Volts DC and no more than 200 mA. This would mean the relay coil resistance will have to be more than 100 ohms. If it is more it will be better as this will put less load on the 555 Timer.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to jw0752

    If my Ohm's Law is correct, wouldn't I need (if using a 12V DC supply) 60 Ohms of coil resistance? Nonetheless here is one I found that may be suitable, possibly overkill (but at least not UK stock.)

     

    HE721A1200 - HAMLIN HE721A1200 - REED RELAY, SPST-NO, 12VDC, 0.5A, THD | Newark element14 US

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    Hi Simon, I really like the way you are researching and checking things out. Your Ohms law is corrent but I do not want the relay to end up drawing the max current that the 555 can deliver without damage. I want the relay to draw mabe half or 100 mA if possible. Also we will loose some of the 12 volt supply inside the 555 timer so the actual voltage on the relay may be 10 or 11 volts. If we have 10 volts and 100 mA then our resistance should be 100 ohms approx. The other consideration when we choose the relay will be the Amp rating on the contacts. I would estimate that 5 amps will be adequate. If the contacts are rated for more, even better. I will try to look at your parts list later.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    Hi Simon, I really like the way you are researching and checking things out. Your Ohms law is corrent but I do not want the relay to end up drawing the max current that the 555 can deliver without damage. I want the relay to draw mabe half or 100 mA if possible. Also we will loose some of the 12 volt supply inside the 555 timer so the actual voltage on the relay may be 10 or 11 volts. If we have 10 volts and 100 mA then our resistance should be 100 ohms approx. The other consideration when we choose the relay will be the Amp rating on the contacts. I would estimate that 5 amps will be adequate. If the contacts are rated for more, even better. I will try to look at your parts list later.

    John