element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Burglar Alarm to Door Buzzer Using a Monostable Circuit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 31 subscribers
  • Views 4414 views
  • Users 0 members are here
  • monostable
Related

Burglar Alarm to Door Buzzer Using a Monostable Circuit

e14 Contributor
e14 Contributor over 11 years ago

At work we are currently using what I suspect is a burglar alarm as a door buzzer. It's inappropriately loud to have buzzing the entire time the door is ajar (from barely open onward), as we're a motel and it's frankly obnoxious. However in order to hear people come in from the basement, it's what the folks in charge decided to use. I would very much like to create a monostable circuit so it buzzes for a small amount of time then turns off until the door is shut again, re-arming the buzzer. The buzzer works using a momentary switch that is pressed when the door is shut and released when the door is open. This switch is connected to what looks like a transformer core, and the device also plugs into our AC outlet.

 

I have looked at circuits online, but even using a few simulators I was unable to produce results like I wanted. Can I have some advice? I'm new to electrical engineering.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +1
    Hi Simon, I have set up a mock up of an improved circuit which allows the door switch to close and remain closed. The components that I have selected for C1 and R1 give a time of approximately 5 seconds…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    This is my preliminary bill of materials. I'm still looking for a relay, and am unsure whether or not the connectors I've listed are acceptable for my application.

     

    D103Z25Z5VF63L6R - VISHAY BC COMPONENTS D103Z25Z5VF63L6R - CAPACITOR CERAMIC, 0.01UF, 50V, Z5V, RADIAL | Newark element1…

    ECQ-E2335JB - PANASONIC ELECTRONIC COMPONENTS ECQ-E2335JB - CAPACITOR FILM, 3.3uF, 250V, 5%, RADIAL | Newark element14 U…

    ECA-1VM471 - PANASONIC ELECTRONIC COMPONENTS ECA-1VM471 - CAPACITOR ALUM ELEC, 470UF, 35V, 20%, RADIAL | Newark element1…

    MCMFF04FF2001A50 - MULTICOMP MCMFF04FF2001A50 - RESISTOR, METAL FILM, 2KOHM, 400mW, 1% | Newark element14 US

    MCRE000049 - MULTICOMP MCRE000049 - RESISTOR, CARBON FILM, 10KOHM, 125mW, 5% | Newark element14 US

    1N4148. - MULTICOMP 1N4148. - SMALL SIGNAL DIODE 100V 150mA DO-35 | Newark element14 US

    NE555P - TEXAS INSTRUMENTS NE555P - IC, PRECISION TIMER, SINGLE, 500KHZ, 16V, DIP-8 | Newark element14 US

    PV-CM-S 2,5-6 image - PHOENIX CONTACT PV-CM-S 2,5-6 image - CONNECTOR, PLUG, 1POS | Newark element14 US

    PV-CF-S 2,5-6 image - PHOENIX CONTACT PV-CF-S 2,5-6 image - CONNECTOR, SOCKET, 1POS | Newark element14 US

    SRB22A2BBBNN - CHERRY SRB22A2BBBNN - SWITCH, ROCKER, SPST, 10A, 250V, BLACK | Newark element14 US

     

    The DC wall adapter and receptacle, internal wiring, a breadboard (I don't think I'll etch this) are also on my list but they're probably fairly straightforward. I'm familiar with the 555 timer's ratings so as long as I don't exceed them (voltage, current) I should be fine, correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    D103Z25Z5VF63L6R - VISHAY BC COMPONENTS D103Z25Z5VF63L6R - CAPACITOR CERAMIC, 0.01UF, 50V, Z5V, RADIAL | Newark element1…

    OK

    ECQ-E2335JB - PANASONIC ELECTRONIC COMPONENTS ECQ-E2335JB - CAPACITOR FILM, 3.3uF, 250V, 5%, RADIAL | Newark element14 U…

    OK

    ECA-1VM471 - PANASONIC ELECTRONIC COMPONENTS ECA-1VM471 - CAPACITOR ALUM ELEC, 470UF, 35V, 20%, RADIAL | Newark element1…

    OK

    MCMFF04FF2001A50 - MULTICOMP MCMFF04FF2001A50 - RESISTOR, METAL FILM, 2KOHM, 400mW, 1% | Newark element14 US

    OK  larger mW than necessary and better precission than necessary

    MCRE000049 - MULTICOMP MCRE000049 - RESISTOR, CARBON FILM, 10KOHM, 125mW, 5% | Newark element14 US

    OK

    1N4148. - MULTICOMP 1N4148. - SMALL SIGNAL DIODE 100V 150mA DO-35 | Newark element14 US

    No Get a regular Schottky like a 1N5819 while your choice will work we might as well put in a little heavier duty.

    NE555P - TEXAS INSTRUMENTS NE555P - IC, PRECISION TIMER, SINGLE, 500KHZ, 16V, DIP-8 | Newark element14 US

    OK

    PV-CM-S 2,5-6 - PHOENIX CONTACT PV-CM-S 2,5-6 - CONNECTOR, PLUG, 1POS | Newark element14 US

    PV-CF-S 2,5-6 - PHOENIX CONTACT PV-CF-S 2,5-6 - CONNECTOR, SOCKET, 1POS | Newark element14 US

    OK designer choice.

    SRB22A2BBBNN - CHERRY SRB22A2BBBNN - SWITCH, ROCKER, SPST, 10A, 250V, BLACK | Newark element14 US

    OK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to jw0752

    Thanks for the advice on that diode. I wasn't sure what was considered a standard diode, so I eliminated a few that were obviously not what I was looking for. As for the 2K resistors, they were the cheapest ones so as long as they're ok and available, I'll stick with them.

     

    I found a relay (I could only find 3A ones at Newark) and a power supply that would work with it. I also have 13.5V options for a power supply, I just need a power supply a little over the relay coil's nominal voltage correct?

     

    5501-12-1 - COTO TECHNOLOGY 5501-12-1 - REED RELAY, SPST-NO, 12VDC, 3A, THD | Newark element14 US

    WSU150-0560-R - TRIAD MAGNETICS WSU150-0560-R - AC-DC CONV, EXTERNAL PLUG IN, 1 O/P, 8.4W, 15V | Newark element14 US

     

    and a diode, perhaps C3D02060A - CREE C3D02060A - SIC SCHOTTKY DIODE, 2A, 600V TO-220 | Newark element14 US (all I'm seeing on Newark is UK stock for that part number.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to jw0752

    Thanks for the advice on that diode. I wasn't sure what was considered a standard diode, so I eliminated a few that were obviously not what I was looking for. As for the 2K resistors, they were the cheapest ones so as long as they're ok and available, I'll stick with them.

     

    I found a relay (I could only find 3A ones at Newark) and a power supply that would work with it. I also have 13.5V options for a power supply, I just need a power supply a little over the relay coil's nominal voltage correct?

     

    5501-12-1 - COTO TECHNOLOGY 5501-12-1 - REED RELAY, SPST-NO, 12VDC, 3A, THD | Newark element14 US

    WSU150-0560-R - TRIAD MAGNETICS WSU150-0560-R - AC-DC CONV, EXTERNAL PLUG IN, 1 O/P, 8.4W, 15V | Newark element14 US

     

    and a diode, perhaps C3D02060A - CREE C3D02060A - SIC SCHOTTKY DIODE, 2A, 600V TO-220 | Newark element14 US (all I'm seeing on Newark is UK stock for that part number.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    Hi Simon,

    Check out Newark part # 17M1743  and # 18C9038.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to e14 Contributor

    Keep in mind when getting the power supply for the circuit that the max supply for the 555P is 15 volts. If you go higher than this you will need to incorporate a voltage regulator.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to jw0752

    Yeah, that's why I limited my search to supplies between slightly over 12V to 15V. Thankfully there were several to choose from.