element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum A beginners project kinda need some guidence.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 30 subscribers
  • Views 556 views
  • Users 0 members are here
Related

A beginners project kinda need some guidence.

e14 Contributor
e14 Contributor over 11 years ago

Hey I am trying to make a compact project that isn't to expensive.  Basically I want t reinvent the wheel to some extent and put a digital egg timer into a epipen trainer body.  Realistically I could take a standard count down timer cut it in half, and fold the board over re working the connections.  However I want to learn the basics first, because I have tons more projects I would like to work on.

 

What I am looking to do.

 

1.  Have a kill switch that when pushed in shuts off the device or turns off any lights which will be under the blue cap being depressed by a tab sticking into the body.

 

2.  A display preferably of LEDs in a line that will count down minutes (doesn't really need a second count down. Max of maybe 10 minutes)

 

3.  A noise making speaker for when the device has counted down to zero.

 

4.  A button that when released starts the timer.

 

So basically take off blue back, push the pen against your leg and then have the timer count down.  Once timer is done alarm sounds until you close up the orange tip, or blue back end.

 

epipen10.gif

 

EpiPen_Trainer.jpg

 

I am super beginner on this project and will have lots of questions probably.  We built the device using a adrino UNO kit at a micro-controller meetup group here in Savannah GA, but someone suggested a 555 chip would be simpler and possibly cheaper way to make one.  I plan on making a few of these as well to prototype out.  With that said could anyone kinda guide me in the right direction on this?

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 11 years ago

    You seem to have posted this three times in at least two different groups. Once is enough - you should never multi-post.

     

    Stick with the Arduino - a 555 timer, apart from being just so last century, will not be an economical solution as soon as you want multiple lights, a couple of switches and some logic functions as well as just timing. If you ever mass produced this a simple processor would cost very little more than the 555 and wouldn't need a whole load of support bits and pieces.

     

    If I were working on this I'd go straight in with a custom board using and ARM Cortex M0+ (well sub £0.50 in quantity) but since you describe yourself as a  'super beginner' the Arduino is a good starting point.

     

    There is loads of Arduino stuff on the web  - try googling 'Arduino egg timer' to get started.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 11 years ago

    You seem to have posted this three times in at least two different groups. Once is enough - you should never multi-post.

     

    Stick with the Arduino - a 555 timer, apart from being just so last century, will not be an economical solution as soon as you want multiple lights, a couple of switches and some logic functions as well as just timing. If you ever mass produced this a simple processor would cost very little more than the 555 and wouldn't need a whole load of support bits and pieces.

     

    If I were working on this I'd go straight in with a custom board using and ARM Cortex M0+ (well sub £0.50 in quantity) but since you describe yourself as a  'super beginner' the Arduino is a good starting point.

     

    There is loads of Arduino stuff on the web  - try googling 'Arduino egg timer' to get started.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett

    I only posted this once from what i can tell, but I got a logon error when I tried to post.  Actually I have never posted about this online except that one time.  I will look up the ARM cortex M0+ in the processor maybe one of the micro controller guys will no something, but I will also hit up the arduino egg timer to get started maybe understanding the basics there will soften the learning curve.  If you see this replied more then once let me know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor

    We seem to get a lot of odd error messages  - I can only see one reply.

    The Arduino is easier to start with but there are nice cheap boards form NXP and ST with Cortex M0 processors.

     

    MK